Press Releases
Latest Raspberry Pi 3 computer board now available from RS Components
New Model B+ delivers more processing and faster communications
Australia, 15 March 2018:

RS Components (RS), the trading brands of Electrocomponents plc (LSE:ECM), the global distributor for engineers, today announced availability of the latest Raspberry Pi computer board: Raspberry Pi 3 Model B+. It is now available to order supplied with the official Raspberry Pi case here.
Building upon the phenomenal success of the Raspberry Pi 3 Model B, which will remain in production, the new board is the latest product in the Raspberry Pi 3 range and targets a very wide range of users including students and enthusiasts, as well as experienced engineers and professionals who are developing innovative Internet of Things (IoT) applications.
Raspberry Pi 3 Model B+
The new Model B+ board is based upon the latest revision of the Broadcom BCM2837 System-on-Chip (SoC) processor running at 1.4GHz, more than 10% faster than the processor on the current Raspberry Pi 3 Model B. The BCM2837 processor is a quad-core device that integrates an ARM A53 processor core cluster running the 64-bit ARMv8 instruction set. Multimedia handling capability of the processor includes support for H.264, MPEG-4 decode (1080p30), H.264 encode (1080p30) and OpenGL ES 1.1, 2.0 graphics.
The Model B+ board also offers 1GB of LPDDR2 SDRAM memory and the latest wireless combo chip from Cypress Semiconductor, which provides dual-band 2.4GHz and 5.0GHz Wi-Fi according to IEEE802.11ac, as well as the Bluetooth 4.1 specification for BLE (Bluetooth Low Energy) communications, delivering significantly reduced wireless compliance testing and thereby improving both cost and time to market.
The board also offers improved communications performance via Gigabit Ethernet over USB 2.0, delivering a maximum throughput of 300Mbps through the board’s four USB 2.0 ports; as well as retaining the extensive 40-pin GPIO (General Purpose Input Output) header connector. Audio/video connections include HDMI and MIPI DSI/CSI display/camera ports, as well as a four-pole stereo output and composite video port.
While offering improved thermal management compared to previous Raspberry Pi incarnations, the board also retains many of the same features and capabilities of previous-generation boards such as its small mechanical footprint of 85 x 56mm, making it suitable for the current official Raspberry Pi case, as well as many other third-party enclosures available on the market today.
“Once again, Raspberry Pi continues to evolve, boosting its processing and communications performance,” said Lindsley Ruth, Chief Executive Officer at Electrocomponents. “RS is honoured to continue partnering with the Raspberry Pi Foundation to deliver new capabilities for individual users and businesses looking to develop applications for the IoT, as well as other innovative concepts and designs.”
The Raspberry Pi 3 Model B+ is manufactured exclusively in the UK under licence by the distributor. For further resources, please visit RS Components Raspberry Pi.
A series of articles is published on the DesignSpark website, as follows:
Raspberry Pi 3 Model B vs. 3 Model B+
https://www.rs-online.com/designspark/raspberry-pi-3-model-b-vs-3-model-b
Building a Remote SDR with the Raspberry Pi 3 Model B+ and SDRplay RSP2
https://www.rs-online.com/designspark/building-a-remote-sdr-with-the-pi-3-model-b-and-sdrplay-rsp2
Building custom remote sensing platforms with the Raspberry Pi 3 Model B+
About RS Components
RS Components and Allied Electronics & Automation are the trading brands of Electrocomponents plc, the global distributor for engineers. We offer more than 500,000 industrial and electronic products, sourced from 2,500 leading suppliers, and provide a wide range of value-added services to over one million customers. With operations in 32 countries, we trade through multiple channels and ship around 50,000 parcels a day.
Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2017 had revenues of £1.51bn.
For more information, please visit the website at www.rs-online.com.
Further information is available via these links:
Twitter: @RSElectronics; @alliedelec; @designsparkRS
RS Components on Linkedin
http://www.linkedin.com/company/rs-components
RS WeChat ID: RS_Components_CN
Relevant Links:
Electrocomponents plc
www.electrocomponents.com
RS Components
www.rs-online.com
DesignSpark
http://www.designspark.com