Temperature transmitters serve as a crucial interface between a control device and a temperature sensor These electrical instruments connect seamlessly with temperature gauges, ensuring accurate signal transmission. Essentially, a temperature transmitter converts the signals produced by temperature sensors into standard instrumentation formats.
This process not only measures the temperature but also allows for effective control of the process variable temperature. By doing so, temperature transmitters play a vital role in maintaining optimal conditions in various industrial and commercial applications.
Temperature transmitters take the temperature reading from a sensor and convert it into a standardised output signal. These signals, which usually range from 4-20mA, are then sent over to a controller, which will determine the next line of action. Controllers can be either DCS or PLC. These controllers are used to monitor and control industrial processes, using the temperature data received from the transmitter to make decisions and adjust process parameters accordingly.
Temperature transmitters come in various types, each designed for specific temperature-sensing technologies and applications. Here are some common types:
An RTD transmitter is designed to work with Resistance Temperature Detectors (RTDs). RTDs are temperature sensors that exhibit a change in electrical resistance with temperature. The RTD transmitter measures this resistance change at its input and converts it into a standardised output signal, such as 4-20mA. RTD transmitters are known for their accuracy and stability over a wide temperature range.
RTD transmitters have the following features:
PT100 transmitters (sometimes referred to as PT100 thermocouples or PT100 thermistors) are commonly used in the process industry. They are a form of RTD transmitter and typically have a resistance level of around 320F (100 ohms at 0°C). Whenever the temperature is higher, its resistance is going to be dependent on the particular sensor version.
PT100 transmitters have the following features:
A thermocouple transmitter is designed to work with thermocouples. Thermocouples consist of two dissimilar metals joined together, producing a voltage that varies with temperature. The thermocouple transmitter measures this voltage and converts it into a standardised output signal. Thermocouple transmitters are known for their wide temperature range and ability to withstand harsh environments.
Thermocouple transmitters have the following features:
When selecting a temperature transmitter, it's important to consider its key features to ensure it meets your application requirements.
Accuracy refers to how closely the transmitter's output signal represents the actual temperature being measured. High accuracy is crucial in applications where precise temperature monitoring and control are essential. Look for transmitters with low accuracy errors, typically expressed as a percentage of the span or in degrees Celsius.
Stability refers to the transmitter's ability to maintain its accuracy over time and under varying environmental conditions. A stable transmitter will provide consistent and reliable readings, minimising the need for frequent recalibration.
Response time is the time it takes for the transmitter to react to a change in temperature and provide an updated output signal. Choose a transmitter with a fast response time if your application requires rapid temperature monitoring or control.
Isolation refers to the electrical separation between the input and output circuits of the transmitter. This prevents interference and ground loops, ensuring accurate measurements and protecting connected equipment.
Temperature transmitters are essential components in various industrial processes, providing accurate and reliable temperature measurements for monitoring and control.
In discrete manufacturing, temperature sensor transmitters are used to monitor the temperature of machines, equipment, and processes. This helps ensure optimal operating conditions, prevent overheating, and maintain product quality.
Temperature transmitters are crucial in process manufacturing for monitoring and controlling temperatures in reactors, vessels, and pipelines. They ensure efficient and safe operation of chemical reactions, food processing, and other industrial processes.
In the energy and utilities sector, temperature transmitters monitor the temperature of critical equipment in power plants, refineries, and other facilities. This helps prevent equipment failure, optimise energy efficiency, and ensure safety.
Temperature transmitters are used in facilities and intralogistics to monitor temperature in storage areas, warehouses, and transportation systems. This helps maintain optimal conditions for sensitive goods, prevent spoilage, and ensure product quality.
Selecting the right temperature transmitter is crucial for accurate and reliable temperature measurement in your application. Here are some critical factors to consider:
RS is your reliable source for high-quality industrial temperature transmitters. We stock an extensive range from industry leaders like Endress+Hauser, LKMelectronic, and our own RS Pro line. Our selection spans various types and specifications at competitive prices, ensuring you find the perfect temperature transmitter for your application.
We also carry other essential process components, such as ammeters and digital temperature controllers, to provide comprehensive solutions for your industrial automation and control needs. Order your RTD temperature transmitters, PT100 temperature transmitters and other accessories online today.
We provide dependable delivery from as soon as the next working day. For approved business account customers, delivery is free on all orders over $40. We also welcome offline orders via telephone, email, or fax. For these orders, business account customers with a valid ABN enjoy free delivery on all orders over $80. Convenient self-collection from our Sydney branch is also available.
For more details, please refer to our Delivery Page.