Screened Cable
The popularity of shielded cable, screened cable, and unscreened video cables have grown. This results from reduced cord clutter by shielding, more convenient identification labels, and less noise and interference per wavelength.
Screened cable is a component of almost every data center that is used for the uninterrupted transmission of signals to and from the equipment. The cable is shielded to create a barrier between different signals or components of the same signal.
Screened Cable
Screened cable is an electrical cable with a screen or mesh grid in its insulation. The screen protects against short circuits, open circuits, and ground faults. Screened cable is used in the power industry to carry power through underground, underwater, and aerial applications.
The screens of screened cables have many openings, called "pores", designed to allow electricity passage but not anything else. When you touch a screened cable with your bare hands, you're likely to feel the smooth surface of the screen.
However, these screens can become electrically charged when touched with a conductive object like metal rods. Screened cables are available in three basic types: stranded-screened (SS), multi-strand (MS), and solid-screened (SSS).
Multicore Screened Cable
Multicore Screened Cable is a kind of cable that has a large number of cores. The core comprises many strands, each being connected to the other strands.
The Multicore Screened Cable has many advantages. It can be used in high frequency and low frequency and has good mechanical properties, electrical properties, chemical properties, etc.
Multicore-screened cable is a kind of fiber optic cable that can handle multiple data transmissions in one fiber. This kind of cable has been used for long-distance transmission for many years, especially for large transmission cables. The multicore screened cable consists of several cores of different sizes, which are connected by a special connector.
Features and Benefits
The screened cable is the most widely used cable type because it has a higher voltage rating. A screened cable is typically rated at 5 VDC, although some versions may be rated as high as 100 VDC. The screened cable is also known as multicore or multi-core screened cable.
The major advantage of this type of cable is that it can handle a larger current than standard twisted-pair or coaxial cables. This allows you to use it when the other types would not work, such as when you need to run a high-power device such as an electric guitar amplifier or an electric piano.
Another advantage to using this type of cable is that it can handle more data than standard twisted-pair and coaxial cables. This means that you can use a greater frequency range for your data line than what you could get with standard cabling, which will allow for more channels (or signals) on your networked computer system or networked home entertainment system.
Related links
- Twisted Pair & Multicore Data Cable
- Belden Multicore Industrial Cable, 3 Cores, 0.82 mm², Screened,...
- Belden Twisted Pair Multipair Industrial Cable, 2 Pairs, 0.33 mm²,...
- Control Cable
- Ethernet Cable
- TE Connectivity Straight Female SPE to Straight Male SPE Ethernet...
- Belden Twisted Pair Data Cable, 3 Pairs, 0.2 mm², 6 Cores, 24 AWG,...
- Belden Twisted Pair Data Cable, 1 Pairs, 0.9 mm², 2 Cores, 18 AWG,...