- Published 10 Dec 2024
- Last Modified 10 Dec 2024
- 7 min
Complete Guide to MCBs: Type A, B, C D Circuit Breakers
Our guide to Miniature Circuit Breakers (MCBs) explores what is an MCB in electrical systems and the different types of MCBs.

What Are Miniature Circuit Breakers (MCBs)

Miniature Circuit Breakers (MCBs) are essential safety devices used in nearly all modern electrical system. These electromechanical switches automatically interrupt the flow of electricity in a circuit when they detect a fault, such as an overload or a short circuit.
In Australia, MCBs are critical for ensuring the safety of electrical systems in residential, commercial, and industrial applications. They provide reliable layer of protection against electrical hazards, significantly reducing the risk of electrical fires and equipment damage.
What Is the Importance of MCBs in Electrical Systems
MCBs play a vital role in maintaining the safety and integrity of electrical systems. Their primary purpose is to protect circuits from damage caused by excessive current flow. This protection is critical in two main scenarios:
- Preventing Overloads: An overload is what happens when too many appliances draw current from a single circuit, exceeding its designed capacity. MCBs quickly trip and break the circuit, preventing overheating and potential electrical fires.
- Protecting Against Short Circuits: A short circuit occurs when a live wire comes into contact with a neutral or earth wire. This results in a sudden surge of current that can be extremely dangerous. MCBs instantly detect this surge and trip to isolate the faulty circuit, minimising the risk of electrical shocks or fire.
Compared to traditional fuse types, MCBs offer significant advantages in modern electrical installations. They are resettable, eliminating the need for replacements, and their compact design allows for more circuits to be protected in a smaller space.
How Do Miniature Circuit Breakers Work
MCBs are cleverly designed to respond to different types of electrical faults, using two main operating mechanisms:
- Thermal Operation: For overload protection, an MCB relies on a thermal bimetallic strip. When the current flowing through the MCB exceeds its rated value, the bimetallic strip heats up and bends due to thermal expansion. This bending action triggers a mechanism that trips the MCB, interrupting the current flow and protecting the circuit.
- Magnetic Operation: To handle short circuits, MCBs utilise an electromagnetic coil. When a short circuit occurs, a very high current flows through the coil, generating a strong magnetic field. This magnetic field forces a plunger to move, instantly tripping the breaker much faster than the thermal mechanism.
- Arc Extinguishing: When an MCB trips due to either overload or short circuit conditions, it can generate an electrical arc between contacts. To prevent this arc from causing damage, MCBs incorporate an arc chute. This chamber contains a series of metal plates that cool and split the arc, protecting the surrounding components.
Types of MCB
Miniature Circuit Breakers (MCBs) are categorised into different types, defined by trip curves. These curves illustrate how quickly an MCB will trip in response to an overcurrent. Understanding trip curves is crucial for selecting the appropriate MCB type for specific applications.
Each type (A, B, C, D) has a unique curve that dictates its sensitivity to overcurrents, ensuring that the MCB provides optimal protection without unnecessary tripping.
Type A Circuit Breaker
Type A circuit breakers are the most sensitive. They trip when the current flowing through exceeds the rated current by a small margin:
- Trip Sensitivity: Trips at 2-3 times the rated current.
- Common Applications: Primarily used for highly sensitive electronic equipment, such as semiconductors and circuits with long cable lengths where voltage drops can be a concern.
Type B Circuit Breaker
Type B MCBs offer a moderate level of sensitivity and are the most common type found in domestic or residential installations:
- Trip Sensitivity: Trips at 3-5 times the rated current.
- Common applications: Suitable for protecting general household circuits, including lighting, sockets, and small appliances like refrigerators and washing machines.
Type C Circuit Breaker
Type C MCBs have a higher trip threshold compared to Type B and are designed to handle moderate inrush currents:
- Trip Sensitivity: Trips at 5-10 times the rated current.
- Common Applications: Commonly used in commercial and industrial settings for circuits with inductive loads, such as motors, transformers, and fluorescent lighting.
Type D Circuit Breaker
Type D MCBs are the least sensitive type and are specifically designed to handle very high inrush currents:
- Trip Sensitivity: Trips at 10-20 times the rated current.
- Common Applications: Primarily used in industrial environments for heavy-duty applications, such as large motors, X-ray machines, and welding equipment, where high starting currents are expected.
Overview of MCB Types
MCB Type | Trip Characteristics | Trip Sensitivity (Overload) | Typical Applications |
|---|---|---|---|
| Type A | Extremely sensitive, fast tripping | 2-3 times the rated current | Sensitive electronics, control circuits, medical devices, low inrush current equipment |
| Type B | Standard sensitivity, moderate tripping time | 3-5 times the rated current | Residential circuits, lighting, small household appliances, circuit boards |
| Type C | Moderate sensitivity, handles higher inrush currents | 5-10 times the rated current | Commercial buildings, light industrial, motor circuits, HVAC systems |
| Type D | Least sensitive, designed for high inrush currents | 10-20 times the rated current | Heavy-duty industrial equipment, large motors, transformers, high-capacity machinery |
Poles in MCBs: Single-Pole, Double-Pole & More
In the world of MCBs, "poles" refer to the number of individual circuits that the breaker can protect.
Each pole has a separate set of contacts that can be opened or closed to control the flow of electricity. This allows for different wiring configurations and levels of protection.
- Single-Pole MCB (1P): A single-pole MCB is the most basic type, designed to protect a single live conductor. It is commonly used in domestic settings for lighting circuits and individual socket outlets.
- Double-Pole MCB (2P): A double-pole MCB provides a higher level of safety by isolating both the live and neutral conductors simultaneously. This is particularly important for appliances that require a higher degree of protection, such as water heaters and cookers.
- Three-Pole (3P) & Four-Pole (4P) Options: Available for three-phase applications; these configurations are crucial for industrial settings where three-phase power is utilised for motors or heavy machinery.
Choosing the Right MCB for Australian Applications
Selecting the correct Miniature Circuit Breaker (MCB) is crucial for ensuring electrical safety and compliance with Australian standards. Here are the key factors to consider when determining what MCB is right for your application:
- Circuit Type and Load: Identify the type of circuit you need to protect (lighting, power, etc.) and the total current draw. This will determine the appropriate breaker rating.
- MCB Type (A, B, C, D): Consider the characteristics of the load. For sensitive electronics, Type A is suitable. For household circuits, Type B is common. Type C is better suited for inductive loads like motors, while Type D handles very high inrush currents.
- Number of Poles: Determine how many live conductors need to be protected. Single-pole MCBs are sufficient for most domestic circuits, while double-pole MCBs are necessary for appliances requiring greater isolation.
- Breaking Capacity: This indicates the maximum fault current the MCB can safely interrupt. It should be chosen based on the potential short-circuit current at the installation point, common ratings include 6kA or 10kA depending on application needs.
Compliance with AS/NZS 3000:2018 Standard
In Australia and New Zealand, electrical installations must comply with the AS/NZS 3000:2018 standard, also known as the "Wiring Rules." This standard outlines essential requirements for electrical safety, performance, and installation practices, ensuring that electrical systems are safe and reliable.
When choosing Miniature Circuit Breakers (MCBs), it's crucial to select those that meet the AS/NZS 3000:2018 standard. This ensures that the MCBs have been tested and certified to provide reliable protection against overcurrents and short circuits.
Key Compliance Aspects:
- Certification Marks: Always look for MCBs that carry appropriate certification marks indicating compliance with Australian standards. These marks ensure that the products have been tested for safety and performance.
- Residual Current Devices (RCDs): The AS/NZS 3000:2018 standard mandates the use of RCDs on all final sub-circuits in residential installations. Ensure your MCBs are compatible with RCDs to enhance protection against electric shock.
- Arc Fault Detection: While not a requirement, consider MCBs that incorporate arc fault detection capabilities. These devices can identify arcing conditions that may lead to electrical fires, providing an additional layer of safety.
- Installation Practices: Proper installation is critical for compliance. Ensure that MCBs are installed in accordance with the spacing and clearance requirements outlined in the standard, such as maintaining a minimum clearance of 1 metre around switchboards.
- Regulatory Oversight: Compliance is enforced by various regulatory bodies across states, including Energy Safe Victoria and the Queensland Electrical Safety Office. Familiarise yourself with local regulations to ensure full compliance.
Popular Circuit Breaker Brands
When choosing circuit breakers for Australian applications, it's important to select reputable brands that offer products compliant with AS/NZS 3000:2018. Here are some popular brands known for their quality and reliability:
Schneider Electric
Renowned for high-quality MCBs with extensive ranges suited for residential, commercial, and industrial use in Australia. Schneider Electric MCBs prioritise safety and innovation in their products.
Clipsal Electrical
A popular choice in Australia, Clipsal Electrical MCBs are designed specifically for the local market, ensuring compliance with Australian standards.