- Published 8 Feb 2024
- Last Modified 16 Dec 2024
- 5 min
A Buyer’s Guide to Choosing the Right Digital Multimeter
From safety to accuracy, learn how to choose the right digital multimeter for your electrical work needs. Buy reliable multimeters online at RS Australia.

From installations to maintenance and repairs, precision and safety are key when doing any electrical work. To be precise and safe, electricians use a variety of testing and measuring tools to ensure everything works as intended and hazards are avoided. One of these essential tools is the digital multimeter.
In this guide, we’ll explain what a digital multimeter is, when to use one, and how to choose the right one for your needs.

What is a Digital Multimeter?
A digital multimeter is a device that measures electrical values such as voltage, current, and resistance. In addition to these basic functions, advanced digital multimeters can test diodes and measure capacitance, frequency, and even temperature. The ability to offer multiple measurements with one device makes digital multimeters indispensable in household and professional electrician toolkits.
Unlike analogue multimeters, where a moving needle indicates readings, digital multimeters display measurements on an LCD screen, which provides a precise numerical value. This digital display is easier to read, offers greater accuracy, and has less chance of reading errors compared to the scale and needle system of analog multimeters.
One of the most common use cases of a digital multimeter is to troubleshoot electrical issues within a household. For instance, ensuring a 9V battery is actually delivering 9 volts or testing the continuity of a light switch to confirm it operates correctly.
Now that you’re familiar with a digital multimeter and its uses, let’s take a look at what you need to know before you buy one online.
What to Consider When Choosing a Digital Multimeter?

When selecting a digital multimeter, you can’t just pick any off the shelf. It’s important to understand the tool’s capabilities and ensure they align with your specific electrical tasks. Here are some of the key factors to consider when choosing a digital multimeter, broken down into detail to help you make an informed decision:
1. Capabilities
A digital multimeter’s capabilities determine what it can and cannot measure.
- Voltage and Current: Essential for all electrical work, ensure the digital multimeter is able to accurately measure 240V and 10A, which is the typical voltage range in Australian homes.
- Resistance: Critical for troubleshooting and diagnosing circuit issues. A reliable digital multimeter will provide precise resistance readings, helping you pinpoint problems and ensure circuit integrity.
- True RMS: Some digital multimeters will come with the ability to measure the RMS value of complex or distorted AC waveforms, which is vital for a more accurate representation of power.
- Additional Features: Depending on the complexity of your tasks, you might require additional features like diode testing or capacitance measurement, which can be particularly helpful in more specialised electrical work.
2. Accuracy and Precision
The accuracy of a digital multimeter dictates how close the meter’s readings are to the true electrical value, which is essential for reliable diagnostics. Precision, on the other hand, refers to the repeatability of readings under the same conditions. The accuracy and precision specification of a multimeter is typically expressed as a percentage which represents the potential margin of error in its readings.
For routine household electrical checks, a digital multimeter with moderate accuracy is usually adequate. For professional electrical work, such as working on sensitive electronic circuits, it is better to use models with a lower margin of error.
3. Resolution
A digital multimeter’s resolution is a measure of how detailed the readings can be, reflecting the smallest increment of measurement the device can detect. A multimeter with high resolution can identify subtle fluctuations in electrical values, which is crucial for intricate electrical analysis and fault-finding.
When choosing a digital multimeter, you should select a resolution that balances precision and practicality. While high-resolution multimeters offer more detailed readings, they are more expensive and not always necessary for simpler tasks. For general household electrical work, a multimeter with standard resolution is typically sufficient.
4. Safety Features
Safety features in digital multimeters are critical for both user safety and the longevity of the instrument:
- Overload Protection:nOverlord protection safeguards the multimeter and its users from damage when exposed to currents or voltages beyond its capacity. Look for a multimeter with robust overlord protection in case of accidental high-voltage exposure.
- Compliance with Safety Standards: Multimeters in Australia must adhere to the safety requirements for electrical equipment outlined in AS 61010.1-2003. If you’re looking to buy a digital multimeter online, ensure that this standard is listed under the product description.
Multimeters will often come with a safety category rating, ranging from CAT I to CAT IV. This category rating indicates the level of transient voltage the multimeter can handle. CAT II is typically sufficient for household electrical work, while professional settings involving service lines or high-energy equipment will require a higher category rating for additional safety.
5. Budget Considerations
Last but not least is your budget. Choose a digital multimeter that balances costs with functionality. While affordable options might be attractive, it's crucial to ensure they meet your specific needs. A well-made, feature-rich multimeter can be a valuable long-term investment, especially for complex electrical tasks, offering superior accuracy, reliability, and safety. Investing wisely in a higher-quality multimeter can lead to savings over time, avoiding frequent replacements and ensuring consistent performance for all your electrical work requirements.
Explore Quality Digital Multimeters from RS Australia
Whether you’re performing household electrical checks or complex professional tasks, digital multimeters are essential tools for accurate and efficient electrical troubleshooting. Their ability to simplify complex diagnostics and make electrical jobs easier as well as safer makes them a must-have tool for homeowners and professionals alike.
RS Australia offers an extensive range of digital multimeters and accompanying accessories like multimeter clamps for domestic and industrial applications. Our selection includes products from trusted brands, ensuring you get tools that are reliable, accurate, and compliant with Australian standards. Explore our selection to find the right digital multimeter for your project needs today.
Popular Digital Multimeter Brands
Keysight Technologies
Keysight Technologies provides cutting-edge digital multimeters, known for their innovative features and superior measurement capabilities in various applications.
Related links
- How to Choose the Best Multimeters: Comprehensive Multimeter Recommendations
- Multimeters
- What is a Digital Multimeter & How to Use One
- Multimeter Kits
- Multimeter Leads
- RS PRO RS-9963T Handheld Digital Multimeter True RMS 10 A dc, 1 kV ac
- RS PRO IDM61 Handheld Digital Multimeter
- Amprobe 30XR-A Handheld Digital Multimeter