- Published 22 Feb 2024
- Last Modified 6 Mar 2024
- 5 min
Choosing the Right Flow Meter for Water Management Needs
Discover how to select the ideal flow meter for efficient water management. Explore high-quality flow meter brands like Siemens, Honeywell, & Omron.

Accurate water management is essential in various industrial and commercial sectors, especially in a country like Australia where water resources play a critical role in both urban and rural settings. An integral component of effective water management is the use of flow meters and transmitters, which use sensors to accurately measure the flow of water in various applications. This article delves into the importance, types, and selection criteria of flow meters, ensuring that you make the most informed choice for your specific needs.

What Are Flow Meters?
Flow meters are essential tools in water management, designed to measure the flow rate or volume of water moving through a system. Their applications in Australia span from residential water usage tracking to complex industrial processes. These devices come in various types, each suited for specific environments and requirements. Here's a closer look at mechanical, ultrasonic, and magnetic flow meters and their applications:
Mechanical Flow Meters
Mechanical flow meters are commonly used in residential and commercial settings in Australia. They operate on the principle of a rotating turbine or paddle, which moves in response to water flow. The rotation rate is proportional to the water flow rate, providing a direct measurement. In Australia's residential areas, especially in high-density cities like Melbourne and Sydney, mechanical flow meters are typically used for everyday water usage monitoring. They are favoured for their simplicity and cost-effectiveness, making them a practical choice for household water management.
Ultrasonic Flow Meters
Ultrasonic flow meters use sound waves to measure water flow rates. They are ideal for applications where contact with the water needs to be avoided or where the water contains particulate matter or corrosive elements. In key regions of Australia’s mining industry, such as Western Australia's Pilbara, ultrasonic flow meters are used to manage water flow in processing plants and contribute to sustainable mining practices. They are valuable in these settings for their non-intrusive nature and ability to handle dirty or abrasive water, which is common in mining processes.
Magnetic Flow Meters
Magnetic flow meters, or mag meters, utilise Faraday’s law of electromagnetic induction to measure water flow. They are suitable for applications where the water is conductive or contains a significant amount of solids, such as in Australia’s agricultural sector. They are advantageous for their high accuracy and reliability in measuring the flow of nutrient-rich water in irrigation systems.
How to Choose a Flow Meter?
When selecting a flow meter, several factors should be considered to ensure it meets your specific requirements.
Firstly, consider the water type and quality, as different meters are suited for clean water, wastewater, or other liquid types.
Next, be sure that the flow meter’s flow rate and pressure handling capabilities match your system’s requirements and specifications. This enables accuracy and reliability, especially in industrial settings where precise measurements are critical. Using a flow meter that doesn’t align with system requirements can also potentially damage the flow meter or surrounding system, incurring unexpected costs down the line.
Environmental conditions such as temperature and humidity also play a role in determining the suitable type of meter. A flow meter in the tropical climate of the Northern Territories, for example, has to withstand humidity better than one in Western Australia.
Lastly, consider installation requirements, space limitations, and cost considerations to ensure a practical and cost-effective solution.
Why is it Important to Choose Flow Meters that Comply with Standards?
Adhering to industry standards and compliance requirements is crucial when selecting flow meters. These standards ensure that the meters are safe, reliable, and accurate, which is particularly important in sectors like agriculture and manufacturing, where precise water management is essential. In Australia, where environmental conservation is a priority, choosing a flow meter that meets rigorous standards is a step towards sustainable water usage and management.
Explore RS’ Selection of Flow Meters

In choosing the right flow meter for your water management needs, it’s beneficial to consult with professionals who can provide personalised advice. RS Australia offers a diverse selection of flow meters catering to various industrial and residential needs. Our range of sensor gear includes everything from digital flow meters to ultrasonic flow meters, as well as float switches, inductive proximity sensors, and level sensors, all selected for their quality, reliability, and compliance with water management industry standards.
Popular Water Flow Meter Brands
Related links
- Flow Sensors
- ifm electronic SM2 Series Magnetic Inductive Flow Meter Flow Meter for Water 9600 gph Max
- Flow Meters
- Water Flow Sensors
- pH Meters
- ifm electronic SM7 Series Magnetic Inductive Flow Meter Flow Meter for Water 792 gph Max
- ifm electronic SV Series Vortex Flow Meter Flow Meter for Water 40 L/min Max
- ifm electronic SM7 Series Magnetic Inductive Flow Meter Flow Meter for Water 50 L/min Max