Padlocks are portable and removable locks commonly used for both commercial and residential security. Featuring a shackle that passes through holes, chains, or staples, traditional padlocks consist of a main body, shackle, and internal locking mechanism. Options include standard padlocks, combination models, and smart padlocks, available in various sizes with shackle lengths ranging from 10 mm to 300 mm. They are made from materials like brass, titanium, and stainless steel, with hardened steel used in high-security models for added protection.
Weatherproof padlocks are designed to resist water and corrosion, making them suitable for indoor and outdoor use. Specialty laminated padlocks, often covered in plastic, are ideal for electrical applications due to their superior resistance to chemicals and temperature variations.
Types of Padlocks
- Key Padlocks: Key padlocks require a separate key to lock and unlock the mechanism. Some key padlocks are self-locking, meaning they lock automatically when the shackle is inserted back into the lock.
- Combination Padlocks: Combination padlocks do not use a key. Instead they use a series of wheels which, when aligned correctly, allow the lock to open.
- Smart Padlocks: Smart padlocks, or Bluetooth padlocks, connect to smart devices which can allow access.
- Anti-pick Padlocks: Anti-pick padlocks are designed to be almost impossible to pick and open. This is ideal for extra security.
Key-Lock type padlocks can be divided into two categories:
- Keyed Alike: Uses a single key to open multiple locks. Keying locks alike is a great time-saving solution as, with only one key, time does not need to be spent looking for the correct one. It also saves having to carry around a large bunch of keys.
- Keyed to Differ: Each lock will come with its own key, one which cannot be used on any other locks.
How to Choose the Right Padlock?
To choose the right padlock you need to consider a number of aspects, such as:
- Material: Padlocks are typically made from various metals such as brass, stainless steel and hardened steel. Consider the strength and corrosion resistance needed for your specific application.
- Size and Type: Padlocks come in various sizes and types, including heavy-duty padlocks, combination padlocks and smart padlocks. Ensure that the size of the shackle and the overall size of the padlock fits seamlessly with your application.
- Shackle Diameter: The shackle diameter determines the strength and resistance to cutting. Choose a padlock with a shackle diameter appropriate for the level of security needed. For maximum security, opt for a padlock with a hardened steel shackle.
- Shackle Securing Mechanism: Different padlocks have different shackle securing mechanisms, such as ball bearings or deadbolts. Consider the level of security and pick resistance required for your application.
- Working Environment: Consider whether the lock will be used indoors or outdoors. Outdoor padlocks or those exposed to harsh conditions should be weatherproof and corrosion-resistant.
- Keyed to Differ or Alike: Consider whether you need keyed alike or keyed to differ padlocks. Keyed alike padlocks offer convenience by using the same key for multiple locks, while keyed to differ padlocks provide enhanced security by using unique keys for each lock.
- Value of Assets: The value of the assets being protected should influence your padlock choice. For high-value items, consider a heavy-duty padlock or a combination padlock with enhanced security features.
Key Features to Look for in a High-Quality Padlock
When choosing a padlock, consider these key features:
- Durability: The material of the padlock body and shackle significantly impacts its strength and resistance to damage. Look for padlocks made from hardened steel, stainless steel or other robust materials for effective protection.
- Weather Resistance: If the padlock will be used outdoors or in harsh environments, weatherproof padlocks are essential. Look for features like weatherproof seals, corrosion-resistant materials and drainage holes to prevent moisture damage.
- High-Security Mechanism: The locking mechanism plays a crucial role in the padlock’s security. Seek padlocks with advanced locking mechanisms, such as anti-pick pins or ball bearings, that make it difficult for unauthorised individuals to pick or bypass the lock.
- Cut and Impact Resistance: The shackle should be resistant to cutting and impact to prevent forced entry. Look for padlocks with hardened steel shackles or other robust materials.
- Anti-pick Protection: Anti-pick padlocks are designed to resist picking attempts, making them more difficult to open without the correct key. Look for features like serrated pins, mushroom-shaped shackles and other anti-pick mechanisms.
- Shackle Strength and Size: The shackle's strength and size are crucial for preventing it from being cut or forced open. Choose a padlock with a shackle diameter appropriate for the level of security needed.
- Key Control and Master Key Options: Keyed alike padlocks act as masterkeys that use the same key for multiple locks for convenience, while keyed to differ padlocks have unique keys for each lock, allowing for enhanced security. Consider which one works best for your needs.
- Ease of Use: While security is paramount, the padlock should also be easy to use. Look for features like smooth key insertion, clear markings and ergonomic designs that make it convenient to operate.
How to Maintain and Care for Your Padlock
Proper maintenance and care can significantly extend the lifespan of your padlock and ensure its continued functionality and security. Here are some tips to remember:
- Clean Regularly: Dirt, dust and debris can accumulate in the lock mechanism, hindering its operation. Regularly clean your padlock using a soft brush or compressed air to remove any buildup, avoiding harsh chemicals or abrasive cleaners.
- Lubricate the Lock Mechanism: Lubricating the lock mechanism periodically ensures smooth operation and prevents sticking or jamming. Use a small amount of lubricant specifically designed for locks, such as graphite powder or a silicone-based lubricant. Then, work the key in and out to distribute it evenly.
- Check for Rust and Corrosion: Regularly inspect the padlock for any signs of rust or corrosion, especially if it's used outdoors or in harsh environments. If you notice any rust, clean it off with a wire brush and apply a rust-inhibiting coating.
- Protect from Moisture: If the padlock is used outdoors, ensure it is weatherproof and has adequate protection against moisture. Consider using a protective cover or storing the padlock in a dry location when not in use.
- Test the Key Regularly: Ensure the key operates smoothly in the lock and that the padlock locks and unlocks easily. If you notice any sticking or resistance, lubricate the lock mechanism or consider replacing the key if it's worn or damaged.
- Inspect the Shackle: Regularly check the shackle for any signs of wear, damage or bending. If the shackle is compromised, it could weaken the padlock’s security. Replace the padlock if you notice any significant damage to the shackle.
- Avoid Overloading: Avoid overloading the padlock by using it to secure objects beyond its weight or strength capacity. Overloading can strain the shackle and locking mechanism, leading to premature failure.
- Use a Protective Cover: A protective cover can help shield the padlock from the elements, especially if it's used outdoors. This can prevent damage from rain, snow, UV radiation and other environmental factors.
- Store Keys Safely: Keep your padlock keys in a safe and secure location to prevent unauthorised access or loss. Consider using a key storage box or a designated key rack.
- Replace When Necessary: Even with proper care, padlocks can wear out over time. If you notice any signs of significant wear, damage or malfunction, it's best to replace the padlock to ensure continued security.
Industrial Application of Padlocks
Padlocks are essential security devices used across a wide range of industries, such as:
- Construction Sites: Padlocks are essential on construction sites, securing valuable tools and equipment such as work safety gloves and electric cables, preventing theft and vandalism. Heavy-duty and weatherproof padlocks are particularly vital in Australia due to their ability to withstand harsh conditions and resist tampering.
- Warehouses and Storage Facilities: Padlocks play a crucial role in securing warehouses and storage facilities, protecting valuable inventory and preventing unauthorised access. Combination padlocks and key-operated padlocks are commonly used to secure doors, gates and storage containers.
- Factories and Manufacturing Plants: In factories and manufacturing plants, padlocks are used to secure machinery, control panels and access points, ensuring workplace safety and preventing unauthorised operation. Industrial padlocks with high-security features are often preferred in these settings.
- Railroads and Transportation: Padlocks are used in the transportation industry to secure cargo, equipment and facilities, protecting goods during transit and storage. All weather padlocks and heavy-duty padlocks are essential for withstanding the rigors of transportation environments.
- Energy and Power Plants: Padlocks are crucial for securing energy and power plants, protecting critical infrastructure and preventing unauthorised access to hazardous areas. High-security padlocks and key-lock type padlocks are commonly used in these sensitive locations.
- Oil and Gas Industry: In the oil and gas industry, padlocks are used to secure pipelines, valves and other equipment, preventing tampering and ensuring the safety of operations. Weatherproof padlocks and industrial padlocks are essential for withstanding harsh conditions and potential hazards.
- Public Infrastructure: Padlocks are used to secure public infrastructure, such as bridges, tunnels and water treatment facilities, protecting vital assets and ensuring public safety. Heavy-duty padlocks and weatherproof padlocks are often preferred for these applications.
- Food Processing and Pharmaceutical Industries: Padlocks are used in the food processing and pharmaceutical industries to secure storage areas, control access to production facilities and maintain hygiene standards. Stainless steel padlocks are often preferred in these environments due to their corrosion resistance and hygienic properties.
- Chemical and Hazardous Material Storage: Padlocks play a crucial role in securing hazardous materials, preventing unauthorised access and ensuring safe storage. Specialized padlocks with chemical resistance and corrosion protection are used in these applications.
- Marine and Shipping: Padlocks are used in marine and shipping applications to secure cargo, equipment and access points on vessels and ports, protecting valuable assets and ensuring safety in harsh marine environments. Weatherproof padlocks and corrosion-resistant padlocks are essential for these applications.
Trusted Padlock Manufacturer, Supplier & Distributor in Australia
RS is a reliable provider of padlocks in Australia. We carry a wide range of indoor, outdoor, industrial and heavy-duty weatherproof padlocks from leading brands like ABUS, Brady, Master Lock, and more.
Buy Padlocks Online from RS
Shop padlocks at RS Australia with fast and reliable nationwide shipping. Visit our Delivery Information page to learn more about shipping options and timelines.