- Published 9 Jan 2024
- Last Modified 6 Mar 2024
- 5 min
The Science & Application of Sealants and Adhesives
Sealants and adhesives have applications in almost every field. Learn how surface compatibility, curing techniques and more help optimise their longevity.

Sealants and adhesives play pivotal roles in a myriad of industries, from construction and automotive to electronics and aerospace. In Australia, these substances are particularly crucial in sectors such as marine construction, automotive manufacturing, and the burgeoning renewable energy sector, as they’re essential to creating strong bonds and ensuring watertight seals.
In this comprehensive guide, we explore the science behind how sealants and adhesives work, application techniques, safety considerations, and the crucial roles they play across various sectors in Australia.

Diving Deep into Adhesives
Types of Adhesives and their Applications
Adhesives come in various forms, each tailored to specific applications. Common adhesive types include:
- Epoxies: Epoxies are renowned for their exceptional bonding strength and resistance to heat and chemicals, making them suitable for heavy-duty applications in marine and automotive repairs.
- Cyanoacrylates: Also known as superglues, cyanoacrylates offer rapid curing and strong bonding capabilities for small-scale, precise applications. This makes them commonplace in electronics manufacturing, a thriving industry in Australia.
- Polyurethanes: Polyurethanes combine flexibility with robust bonding capabilities, making them highly versatile in both structural and non-structural applications, including in the residential sector.
Understanding the distinct characteristics of an adhesive layer is crucial in selecting the right type for a particular application.
Factors Influencing Adhesive Selection
In Australia’s varied climate spanning tropical to temperate zones, where environmental factors like UV exposure and humidity are significant, the right adhesive choice is essential. For instance, in applications where surface compatibility is crucial, adhesives that do not react chemically with the materials they are bonding are preferred.
Common considerations to keep in mind include:
- Bond strength: Bond strength determines the adhesive's ability to withstand mechanical stress, making it paramount in applications related to structural integrity.
- Setting time: An adhesive’s setting time can directly influence work efficiency and project timelines, potentially resulting in costly delays if not properly accounted for.
- Environmental resistance: Resistance to environmental factors like humidity, temperature, UV exposure, or solvent exposure will determine how your adhesive lasts in day-to-day use or harsh conditions.
Surface Preparation and Application Techniques for Adhesives
The effectiveness of an adhesive is greatly influenced by how well the surface is prepared, especially in Australia's varied climate. Surfaces should be clean and free of oils or debris for optimal adhesion. In some cases, surface roughening may be necessary to enhance the bond.
The application technique, including the amount and distribution of the adhesive layer, also significantly impacts the final bond strength and durability. For long-lasting results, users should always understand and follow the manufacturer's guidelines for adhesive application and curing.
Exploring the World of Sealants

Types of Sealants and their Applications
Sealants are versatile materials used to close gaps and protect joints in order to prevent the ingress of air, water, or dust. Common sealant types include:
- Silicone sealants: Silicone sealants offer excellent flexibility and weather resistance, making them ideal for outdoor and high-moisture applications such as residential and commercial construction.
- Acrylic sealants: Acrylic sealants are known for their paintability and ease of adhesion to a wide range of surfaces, leading to their popularity in indoor applications such as the burgeoning Australian home renovation market.
- Polyurethane sealants: Polyurethane sealants offer a robust solution for both indoor and outdoor uses due to their strong adhesive properties and resistance to wear.
Choosing the Right Sealant
Selecting the right sealant involves considering its flexibility, adhesive properties, and resistance to environmental factors like UV rays and temperature changes. A sealant being used outdoors in the Northern Territories, for example, should be able to withstand the changing humidity of the regular monsoon seasons in order to maintain its longevity.
The surface compatibility of the sealant is also vital, as it must adhere well without damaging the surface. Flexibility is another key consideration for surfaces that experience movement or expansion, ensuring that the seal remains intact over time.
Proper Application and Curing of Sealants for Effective Sealing
Gauging how long do sealants last will depend on the properties of the substance, the precision of the application process, and of course, the uniquely Australian environmental condiitons it’s grappling with.
Applying the right amount, ensuring even distribution, and smoothing the sealants to create a uniform adhesive layer are key steps for correct application.
As the curing process varies between different types of sealants, users should always follow the instructions provided by the manufacturer. Some sealants may cure upon exposure to air, while others might require specific environmental conditions. Additional aspects such as joint design, tooling, and finishing also contribute to your sealant’s adhesive properties and longevity.
Safety and Environmental Considerations
Safe Handling and Storage of Adhesives and Sealants
In Australia, adherence to safety regulations, such as the Safe Work Australia guidelines, is crucial for the handling and storage of adhesives and sealants. This includes proper labelling, storing in appropriate conditions to prevent degradation, and following safety guidelines for use and disposal.
Health Impacts and Environmental Concerns
Awareness of the health impacts of adhesives and sealants, particularly the VOCs they contain, is critical. The use of PPE clothing and adherence to Australian safety standards during application and curing is mandatory in professional settings. Additionally, on a positive note, awareness of these factors is driving the development and use of products with lower VOC content and more environmentally friendly compositions.
Innovations and Trends in Eco-friendly Products
The Australian market is seeing a shift towards sustainable and eco-friendly adhesives and sealants. Innovations include bio-based adhesives, water-based formulas, and products with reduced toxicological profiles have also emerged in recent years, aligning with the country's growing focus on environmental sustainability and the preference for products with a lower ecological footprint.
Secure the Adhesives and Sealants You Need at RS
Adhesives and sealants are indispensable components in numerous industries throughout Australia, ensuring durability, functionality, and structural integrity. Familiarising yourself with the science behind these materials, coupled with informed product selection and proper application techniques, plays a pivotal role in achieving successful outcomes.
RS provides a wide array of adhesives, glues, sealants, electrical tapes, and other substances suitable for all types of industrial and personal applications. Whether you're in construction, manufacturing, or any other sector, look to RS today to discover your next partner in industrial equipment.
Popular Sealant and Adhesive Brands
TE Connectivity
TE Connectivity specialises in advanced adhesive and sealant solutions, catering to complex industrial requirements. Their products are acclaimed for their precision and durability, affirming TE Connectivity's position as a leader in the Australian industrial sector.
Araldite
Araldite is renowned for its high-performance epoxy adhesives, catering to intricate and demanding applications in the Australian market. Celebrated for its strong bonding capabilities and durability, Araldite adhesives are a preferred choice in sectors requiring precision and long-lasting adhesion.