Recently searched

    WiFi Antennas

    A WiFi antenna is a device built to pick up the wireless network radio transmissions that are broadcasted from several devices such as laptops, routers or mobile phones. They are key components that are needed to pick up or radiate WiFi signals where needed. Antennas come in various forms, including external WiFi antennas that can be mounted externally for improved signal reception and high-gain WiFi antenna that offer increased signal strength and range.

    Consider a WiFi antenna to upgrade your home office or office router where you may be experiencing connectivity issues or are looking to extend the signal of your router. High-gain external WiFi antennas can significantly improve signal quality and coverage, especially in larger spaces or areas with obstacles. For desktop computers, a high-gain WiFi antenna for PCs can enhance wireless connectivity and provide a more stable internet connection. Additionally, antenna upgrades can sometimes be simpler and more cost-effective to fix with a new antenna, especially with home networks.

    How WiFi Antennas Work

    WiFi antennas work by converting electrical signals into radio waves, which are then transmitted wirelessly. When receiving a signal, the antenna captures the radio waves and converts them back into electrical signals that can be processed by the device. The antenna's design and characteristics determine its ability to efficiently transmit and receive signals, affecting the range and quality of the wireless connection.

    Types of WiFi Antennas

    WiFi antennas come in different types, each designed for specific applications and signal coverage requirements. Choosing the right type of wireless Internet antenna is crucial for optimising wireless network performance. Here are the common types:

    Omnidirectional Antennas

    These WiFi antennas focus energy in a 360-degree pattern. This type of antenna is used when coverage in all directions is required. Antennas in this design typically have gain ratings of between 2.2dBi and 14dBi. This means that the antenna amplifies the signal strength in all directions by a certain factor, with higher dBi values indicating greater amplification.

    Directional Antennas

    Directional antennas provide a stronger pattern in a specific direction by focusing the RF wave to provide a great coverage distance. They are often used for point-to-point connections or to extend the range of a wireless network in a specific direction. Common types include Yagi antennas and parabolic antennas, which offer higher gain compared to omnidirectional antennas.

    Semi-Directional Antennas

    These WiFi antennas offer a balance between omnidirectional and directional coverage, providing a wider beamwidth than directional antennas but with some focus in a particular direction. They are often used in scenarios where a broader coverage area is needed with some emphasis on a specific direction.

    Sector Antennas

    Sector antennas provide a focused beam of coverage in a specific sector, typically 90 or 120 degrees. They are often used in outdoor wireless deployments to provide coverage to a specific area, such as a campus or public space.

    How Antenna Patterns Affect Performance

    The antenna pattern refers to the directional characteristics of the antenna, indicating how it radiates or receives signals in different directions. The antenna pattern affects the coverage area and signal strength of the wireless network. Omni-directional antennas provide 360-degree coverage, while directional antennas focus the signal in a specific direction, offering greater range and signal strength in that direction.

    Wavelengths & Frequencies of WiFi Aerial

    WiFi aerials operate on specific wavelengths and frequencies within the radio frequency (RF) spectrum. The most common frequencies used for WiFi are 2.4 GHz and 5 GHz. The 2.4 GHz band offers a longer range and better penetration through obstacles, while the 5 GHz band provides higher speeds and less interference. The choice of frequency depends on the specific application and the desired balance between range and speed.

    Importance of Using Wireless Antenna

    WiFi antennas, especially high-gain antennas, are able to:

    • Enhance Signal Strength: WiFi antennas amplify the signal strength of wireless networks, improving connection quality and reliability.
    • Extend Coverage Range: Wireless antennas extend the coverage range of a wireless network, allowing devices to connect from greater distances.
    • Improve Signal Quality: WiFi antennas improve signal quality and reduce interference, leading to a more stable connection.
    • Increase Data Transfer Speeds: High-gain WiFi antennas can improve data transfer speeds by enhancing signal strength and reducing errors.
    • Support Multiple Devices: WiFi antennas can help support a larger number of devices connected to a wireless network.

    Applications of WiFi Antennas

    WiFi antennas are used in a wide range of applications across various industries, including:

    Discrete Manufacturing

    In discrete manufacturing, WiFi antenna enable wireless communication between machines, sensors, and control systems, facilitating automation and data collection on the factory floor.

    Process Manufacturing

    WiFi antennas are used in process manufacturing to monitor and control process parameters remotely, improving efficiency and safety in hazardous or difficult-to-access areas.

    Energy & Utilities

    WiFi antennas enable wireless communication in energy and utility applications, such as smart grids and remote monitoring of infrastructure, improving efficiency and reliability.

    Facilities & Intralogistics

    WiFi antennas support wireless communication in warehouses, distribution centres, and other facilities, enabling efficient inventory management, tracking of goods, and automation of material handling processes.

    How to Choose the Suitable Wifi Antenna

    Choosing the right WiFi antenna depends on several factors, including:

    • Coverage Area: Consider the desired coverage area and whether you need omni-directional or directional coverage.
    • Gain: Higher gain WiFi antennas provide stronger signals and longer range.
    • Frequency: Choose the appropriate frequency band (2.4 GHz or 5 GHz) based on your needs.
    • Connector Type: Ensure the antenna connector is compatible with your device.
    • Environmental Conditions: Consider factors like weather resistance for outdoor installations.

    Regulatory Considerations for External WiFi Antennas

    In Australia, the use of external WiFi antennas is subject to regulatory compliance. It is important to ensure that the antenna and its installation comply with the relevant regulations and standards set by the Australian Communications and Media Authority (ACMA). This includes adhering to power output limits and ensuring the antenna does not cause interference with other radio communication services.

    Trusted Internet Antenna Manufacturer, Supplier & Distributor in Australia

    RS is your reliable source for high-quality WiFi antennas. We stock an extensive range from industry leaders like Linx, Mobilemark and Molex. Our selection of WiFi and Internet antennas spans various types and sizes at competitive prices, ensuring you find the perfect antenna for your application.

    We also carry other essential networking components, such as computer cables and ethernet connectors, to provide comprehensive solutions for your connectivity needs. Buy WiFi antennas for PCs, high-gain WiFi antennas, and other accessories online today.

    Buy High-Gain WiFi Antennas Online from RS

    We provide dependable delivery from as soon as the next working day. For approved business account customers, delivery is free on all orders over $40. We also welcome offline orders via telephone, email, or fax. For these orders, business account customers with a valid ABN enjoy free delivery on all orders over $80. Convenient self-collection from our Sydney branch is also available.

    For more details, please refer to ourDelivery Page.

    1 of 1
    Results per page

    Popular Searches