Recently searched

    Pozidriv Screwdrivers

    The Phillips drive concept has been enhanced with the Pozidriv, which is sometimes spelt mistakenly as "Pozidrive." The Pozidriv design was developed by the business GKN Screws & Fasteners when the Phillips head patent expired.

    What exactly is a Pozidriv Screwdriver?

    The Pozidriv drive type was created initially to combat cam-out, which is the biggest problem Phillips heads are prone to. When torque reaches a specific level, cam-out refers to the sliding out of a driving recess. The Pozidriv drive style enhances the following two aspects while maintaining the Phillips drive type's self-centering design:

    • It will be able to increase the torque, without any cam-out
    • It will be able to offer better engagement of surface contact in between the recess in faster head and the driver. As a result, it wouldn't be easy to slip upon correct installation.

    Is it possible for you to use a Pozidriv on a Philips screw?

    Although theoretically possible, we do not advise putting the incorrect drive type on a screw. When employing the proper size, a Phillips drive type may be reasonably inserted into a Pozidriv drive recess. It is crucial to remember that even though the Phillips does fit firmly into the driving recess but is still much more prone to strip and cam-out than if you use the appropriate driver.You may also try to extract a Phillips screw using a Pozi driver, but they do not fit as tightly and are far more likely to fall out or harm the recess while being removed. If you are looking forward to purchasing a Pozi screwdriver, you can find few great options available in our store. All you have to do is to browse through the collection and pick the best one that can cater to your needs.

    Where will you be able to use a Pozi screwdriver?

    Although they aren't nearly as common as regular Phillips screws, Pozidriv screws may be utilized almost anyplace. The Torx and Robertson drive types, among many others, have shown to be more dependable than just the Phillips drive style in avoiding cam-out and stripping over time. Because of competing drive type designs, the Phillips drive is beginning to lose favor for manual applications even if it is still immensely common in production because to its self-centering design.

    What are the benefits of using a Pozi screwdriver?

    The key advantage of adopting the Pozidrive over the Phillips drive type is the improved torque even without increased danger of cam-out. Screws with a pozidriv drive can withstand a lot higher torque in the fastener recesses than screws with a Phillips drive.Browse through our store and you will be able to buy the best PZ screwdriver that can help you with your needs.

    4 of 4
    Results per page