Fire Bells & Security Surface Mount Buzzers
Life safety has relied on fire bells for many years. As well as saving countless lives, they have also been used in school attendance systems, temporary security measures, and even as the "Probably the loudest alarm clock in the world."
A fire bell or a security surface mount buzzer is used to alert people to an emergency or security situation.
People are usually alerted through fire bells when a fire occurs in a building. An alarm system or manual pull station activates them, and they are often mounted on the ceiling or wall. In order to attract attention and alert people to evacuate, fire bells emit a loud, continuous ringing sound.
Surface mount buzzers alert people to security events such as break-ins or intruders. They are similar to fire bells. A motion detector or other security system often activates them in residential and commercial settings. Intruders are alerted by loud, continuous buzzers or short, repeated beeps from surface-mount buzzers.
Typically, surface-mount buzzers and fire bells are mounted in a visible location to allow them to be easily heard and seen.
Types of surface mount buzzers
1. Firebells
A firebell, also known as a fire alarm or smoke detector, detects the presence of fire or smoke and alerts people within the building to evacuate. A smoke or heat sensor triggers a loud alarm when it detects smoke or heat. As a safety feature in homes and buildings, firebells can aid people in evacuating quickly and safely in case of fire.
2. Security bell
An alarm bell, also known as a doorbell or door chime, alerts people inside a building when someone approaches the front door. When a visitor presses a security bell, a chime or other audible signal is activated inside the building. It is important to use security bells in order to alert people when a visitor enters the building and to prevent burglars from entering.
3. Electronic sounder
Typically used as an alert or warning device, an electronic sounder produces an audible signal. The most common applications for electronic sounders are fire alarms, security systems, and industrial process control. In response to a particular event or condition, they can be activated manually or automatically.
4. Electromagnetic
In this type of buzzer, magnets, solenoids, oscillators, housings, vibration diaphragms, and magnets combine to create a buzz. Upon receiving the power supply, a magnetic field will be generated by the oscillator that produces the audio signal.
How to choose a surface mount buzzer ?
It is important to consider a number of factors before choosing a surface mounted buzzer or firebell.
- Product size
- Current consumption
- Terminal type
- Frequency Voltage
- Number of volumes
- Type
- Voltage AC/DC
- The tone is Continuous/Pulsed
- Surface Mounting, Leads, and Pins
- The output of sound
- Feedback Option
- Elements of piezoelectricity
Firebells & security surface mount buzzers
Hence, this datasheet summarizes surface buzzer functions, types, circuits, advantages, disadvantages, and where to buy surface mount buzzers and firebells. It consists of electromechanical, electromagnetic, mechanical, piezoelectric, electroacoustic audio signaling devices. An oscillating circuit or audio signal source is used in order to make this buzzer work. Pushing a switch will result in a ring, beep, or click.