• Published 19 Feb 2025
    • Last Modified 19 Feb 2025
  • 9 min

A Comprehensive Guide to Thermometer Calibration

This guide explores various methods for calibrating a thermometer, including digital, probe and infrared thermometers and why it's essential.

RS marketing banner

Thermometer calibration is the process of ensuring your thermometer is reading temperatures accurately. This is crucial for various applications, from scientific research and industrial processes, to ensuring food safety and complying with Australian standards like the Food Standards Code (FSANZ). Calibrating your thermometer helps maintain accuracy, prevent errors and ensure reliable temperature readings for informed decision-making.

A Comprehensive Guide to Thermometer Calibration

Importance of Thermometer Calibration

Thermometer calibration is critical for various reasons, including:

Ensuring Accuracy

Accurate temperature readings are essential across a wide range of applications, such as:

  • Food Safety: In the food industry, accurate thermometers are crucial to prevent undercooking or improper storage temperatures, ensuring food safety and preventing foodborne illnesses.
  • Industrial Processes: Precise temperature control is vital in industrial processes to maintain product quality, optimise efficiency and prevent costly errors or equipment damage.
  • Healthcare: Accurate thermometers are essential in healthcare for monitoring patient health, ensuring the sterility of medical equipment and providing reliable data for diagnosis and treatment.

Regulatory Compliance

In Australia, compliance with food safety regulations is paramount. The FSANZ mandates the use of accurate thermometers in food handling and processing to prevent foodborne illnesses. Additionally, the AS 2853 standard outlines requirements for temperature measurement equipment used in various industries, ensuring accuracy and traceability to national standards.

Minimise Risks

Inaccurate temperature readings can lead to a range of risks and consequences across various fields, including:

  • Food Handling: Inaccurate readings in food handling can result in food poisoning or spoilage, posing a risk to public health.
  • Industrial Processes: In industrial processes, inaccurate measurements can lead to product defects, equipment damage or even safety hazards, impacting productivity and potentially causing harm.
  • Healthcare: In healthcare, incorrect temperature readings can have serious consequences, including misdiagnosis, improper treatment and compromised patient safety.

How to Calibrate a Thermometer

While the specific processes may vary depending on the type of thermometer being used, there are some general steps and best practices that apply to most calibrations.

Ice Point Method (0°C)

The ice point method, also known as the freezing point method, is a common and relatively simple way to calibrate a thermometer. This method is suitable for calibrating digital thermometers, probe thermometers and some types of analogue thermometers. It involves comparing the thermometer’s reading to the known freezing point of water, which is 0°C.

Tools Required:

  • A container (e.g., a glass or beaker)
  • Crushed Ice
  • Water
  • Your Thermometer

How to Calibrate:

  1. Fill the container with crushed ice.
  2. Add enough water to create a slushy mixture, ensuring the ice is fully submerged.
  3. Insert the thermometer probe or sensor into the ice water mixture, ensuring it's not touching the sides or bottom of the container.
  4. Wait for the temperature reading to stabilise.
  5. Compare the thermometer’s reading to 0°C. If the reading is inaccurate, adjust the thermometer according to the manufacturer's instructions until it displays 0°C.
  6. Repeat the test to ensure the thermometer is accurately calibrated.

Boiling Point Method (100°C)

The boiling point method is a common way to calibrate thermometers, especially those frequently used to measure high temperatures. This method is suitable for calibrating probe thermometers and some types of analogue thermometers. It involves comparing the thermometer's reading to the known boiling point of water, which is 100°C at standard atmospheric pressure.

Tools Required:

  • A Container (e.g., a pot or beaker)
  • Water
  • Heat Source (e.g., a stove or hot plate)
  • Your Thermometer

Calibration Steps:

  1. Fill the container with water and heat it to a rolling boil.
  2. Insert the thermometer probe or sensor into the boiling water, ensuring it's not touching the sides or bottom of the container.
  3. Wait for the temperature reading to stabilise.
  4. Compare the thermometer's reading to 100°C. If the reading is inaccurate, adjust the thermometer according to the manufacturer's instructions until it displays 100°C.
  5. Repeat the test to ensure the thermometer is accurately calibrated.

Note: The boiling point of water can vary slightly depending on altitude and atmospheric pressure. If necessary, adjust the expected boiling point based on your location and conditions.

Reference With Calibrated Thermometer

For those seeking a more precise calibration method, referencing a calibrated thermometer is recommended. This method involves comparing the readings of the thermometer being calibrated to a known, calibrated thermometer, and is suitable for calibrating digital, probe and infrared thermometers.

Tools Required:

  • A Calibrated Thermometer
  • A Substance With a Stable Temperature (e.g., a water bath)
  • Your Thermometer

Calibration Steps:

  1. Ensure the substance you're using has a stable and uniform temperature.
  2. Place both the calibrated thermometer and the thermometer you're calibrating into the substance, ensuring their probes or sensors are at the same depth and not touching the sides of the container.
  3. Wait for the temperature readings on both thermometers to stabilise.
  4. Compare the readings. If there is a discrepancy, adjust the thermometer you're calibrating according to the manufacturer's instructions until its reading matches the calibrated thermometer.
  5. Repeat the test to ensure accurate calibration.

Calibrating Probe Thermometers (Dial / Digital)

Calibrating Probe Thermometers (Dial / Digital)

Probe thermometers, including both dial and digital types, are widely used for measuring temperatures in various applications, from cooking and food safety to industrial processes and scientific experiments.

These thermometers typically consist of a probe or sensor attached to a display unit that provides the temperature reading. This includes thermocouple probes, which are often used for specialised applications requiring high-temperature measurements.

Calibration of probe thermometers can be done using either the ice point method or the boiling point method. However, there are some specific considerations for probe thermometers, such as:

  • Response Time: Allow sufficient time for the probe to reach thermal equilibrium with the substance being measured before taking a reading.
  • Immersion Depth: Ensure the probe is immersed to the correct depth as indicated by the manufacturer. Insufficient immersion can lead to inaccurate readings.
  • Stirring: Stir the substance gently to ensure uniform temperature distribution around the probe.
  • Probe Condition: Check the probe for any damage or contamination that could affect the readings.

To adjust a probe thermometer, it’s best to refer to the manufacturer's instructions. Some thermometers have an adjustment screw or nut that can be turned to calibrate the reading. Others may have a digital calibration function that allows for adjustments through the display unit.

Calibrating Kitchen Cooking Thermometers

Kitchen cooking thermometers, also known as food thermometers, are essential tools for ensuring food safety. They help cooks accurately measure the internal temperature of food, preventing undercooking or overcooking. This is crucial for preventing foodborne illnesses and ensuring food is cooked to the appropriate temperature for optimal quality and taste.

Calibration of kitchen cooking thermometers can be done using either the ice point method or the boiling point method. Here are some practical tips on how you can calibrate these thermometers:

  • Probe Cleanliness: Do ensure the probe is clean and dry before and after each use to prevent contamination and inaccurate readings.
  • Immersion Depth: Insert the probe into the thickest part of the food, ensuring it reaches the center without touching bone or fat.
  • Waiting Time: Allow sufficient time for the thermometer reading to stabilise before recording the temperature.
  • Calibration Frequency: Calibrate your kitchen thermometer regularly, especially if it's dropped or exposed to extreme temperatures.

To adjust a kitchen cooking thermometer, refer to the manufacturer's instructions. Some models have a calibration nut that can be adjusted using a wrench or pliers. Others may have a digital calibration function accessible through buttons on the device.

Calibrating Infrared and Laser Thermometers

Calibrating Infrared and Laser Thermometers

Infrared thermometers, also known as laser thermometers, are non-contact temperature measurement devices that use infrared technology to determine the temperature of an object or surface. They are widely used in various industries and applications, from manufacturing and maintenance to healthcare and food safety, due to their ability to measure temperature quickly and without physical contact.

Calibration with a Blackbody Calibrator

While the ice point or boiling point methods can also be used, for industrial applications where high accuracy is critical, calibrating an infrared (IR) thermometer with a blackbody calibrator is recommended. A blackbody calibrator is a device that emits a known and stable infrared temperature, which provides you with a reliable reference for calibration.

Steps:

  1. Set the blackbody calibrator to a specific temperature within the range of the laser thermometer.
  2. Allow the calibrator to stabilise at the set temperature.
  3. Aim the infrared thermometer at the calibrator's target surface, ensuring the distance and angle are within the manufacturer's specifications.
  4. Compare the thermometer’s reading to the calibrator's set temperature.
  5. If the readings differ, adjust the infrared thermometer’s calibration settings according to the manufacturer's instructions until the readings match.

Practical Tips:

  • Ensure the calibrator's target surface is clean and free from any obstructions.
  • Maintain a consistent distance and angle between the thermometer and the calibrator throughout the calibration process.
  • Avoid ambient temperature influences by performing the calibration in a stable environment.

To make any changes, do refer to the thermometer’s user manual for specific instructions on how to calibrate the device. Some models may have buttons or dials for adjustment, while others may require specialised software or tools.

When To Calibrate Thermometer

While the frequency of calibration can vary depending on the type of thermometer and its usage, there are some general signs and scenarios that indicate it might be time for recalibration.

  • Visible Damage: If the thermometer has been dropped, exposed to extreme temperatures or shows any signs of physical damage, it's crucial to recalibrate it to ensure accuracy.
  • Inconsistent Readings: If you notice inconsistent or erratic readings from your thermometer, it's a sign that it may need calibration. Compare its readings to another calibrated thermometer or a known temperature standard to confirm any discrepancies.
  • Extended Periods of Storage: If a thermometer has been stored for an extended period, it's recommended to calibrate it before use to ensure accuracy.
  • Manufacturer Recommendations: Always refer to the manufacturer's instructions for specific calibration recommendations and frequency. Some thermometers may require calibration after a certain number of uses or after a specific time interval.
  • Regulatory Requirements: In some industries, such as food processing or pharmaceuticals, regulatory compliance may mandate regular calibration of thermometers at specific intervals.

How Often to Calibrate Thermometers

The frequency of thermometer calibration depends on various factors, including the type of thermometer, its usage and the required accuracy level. Here are some general guidelines:

  • Daily Use: If you use your thermometer multiple times a day, it's recommended to calibrate it at the start of each day.
  • Regular Use: For thermometers used regularly but not daily, calibrate them weekly or monthly, depending on the required accuracy and the manufacturer's recommendations.
  • Infrequent Use: If you use your thermometer infrequently, calibrate it before each use or at least every few months to ensure accuracy.
  • Critical Applications: In critical applications where precise temperature readings are essential, such as in medical or scientific settings, more frequent calibration may be required, potentially daily or even before each use.

Always refer to the manufacturer's instructions for specific calibration recommendations and adjust the frequency based on your usage and the criticality of the application.

Calibration Certificates in Australia

Calibration Certificates in Australia

In certain industries, maintaining accurate temperature measurements is not only important for quality and efficiency, but also for compliance with regulations and national standards. These industries often require calibration certificates as proof that their thermometers have been calibrated to a recognised standard.

Industries that commonly require calibration certificates include:

  • Food Processing and Handling
  • Pharmaceuticals
  • Healthcare
  • Manufacturing
  • Scientific Research
  • Aerospace

In Australia, the National Association of Testing Authorities (NATA) provides accreditation to calibration laboratories that meet specific quality and competency standards. Calibration certificates obtained from NATA-accredited laboratories are widely recognised and accepted as proof of measurement accuracy and traceability.

RS Australia offers a wide range of high-quality thermometers for various applications, from industrial temperature monitoring to food safety. We partner with trusted brands like Fluke and Testo to provide durable and precise thermometers that meet your needs.

Explore our selection online, add your chosen thermometer to your cart and proceed through our secure checkout. We offer various payment options and fast delivery across Australia, with options to suit your timeframe and budget.

We also provide a variety of other types of products — including Mitsubishi programmable controllers and the fastest ethernet cables — to cater for all your needs. For detailed information on delivery services and costs, please visit our Delivery Information page today. Ensure accurate temperature measurement with a quality thermometer from RS Australia — order yours today!

Related links

Be the first to know about our latest products and offers

Email address

The personal information you provide to us when signing up to this mailing list will be processed in line with the Privacy Policy