- Published 22 Feb 2024
- Last Modified 6 Mar 2024
- 5 min
Mastering Cable Management: A Guide to Using Clips and Clamps
Transform your space with RS Australia’s expert cable management guide. Learn to use cable clips and clamps for a safer, organised, and efficient area.

In Australia, factors like the growing population, booming construction sector, and escalating demand for electricity have collectively led to an increase in the use of wires and cables. This surge is particularly evident in modern living and working spaces, where technology is integral to daily life.
Australian households and workplaces are now more than ever equipped with various electronic devices, from computers and televisions to industrial machinery. While beneficial, the abundance of technology introduces the intricate task of managing a multitude of cables. Without proper organisation, these cables can disrupt the aesthetic of a space and present safety risks.
This comprehensive guide explores the crucial role of cable clips and clamps in creating orderly and hazard-free environments.

Understanding Cable Clips and Clamps
Cable clips and clamps are made for secure cable organisation. Their designs, such as U-shaped or circular clips, are adept at adhering to various surfaces, while clamps efficiently bundle multiple cables, often using ratchet mechanisms for tightening.
Furthermore, these tools are instrumental in preventing cable entanglement, thereby extending cable life and reducing safety hazards like tripping. Their use also enhances the aesthetic appeal of settings, promoting a cleaner, more professional look.
Types of Cable Wire Clips and Clamps:
- Plastic Clips: Lightweight and versatile, they are ideal for everyday cable management.
- Metal Clamps: Durable and robust, suitable for heavier cables or outdoor use.
- Adhesive Cable Clips: These are easy to install without damaging surfaces, making them perfect for temporary setups or rented spaces.
- Nail-In Types: Provide a more permanent solution, best for areas where cables are only moved occasionally.
- Steel Cable Clamps: Excellent for heavy-duty applications, providing secure holding power in industrial or high-stress environments.
How to Choose the Right Cable Clips and Clamps
Selecting the right cable clips and clamps involves several key considerations:
Cable Types and Load
Opt for robust clamps like steel or metal for larger, heavier bundles. In contrast, plastic or adhesive-backed cable clips are sufficient for lighter office or home use, such as managing computer cables or small appliances.
Surface Compatibility
Nail-in types are suitable for permanent installations on sturdy surfaces like concrete or metal. On the other hand, adhesive-backed and rubber clips provide a secure yet damage-free option for applications like desk cable management, where surfaces are often made of wood.
Aesthetic and Functional Balance
While industrial or commercial settings prioritise functionality, maintaining a professional look is still important. Choose cable management solutions that are both effective and unobtrusive. For home settings, where aesthetics might be more crucial, select clips and clamps that blend seamlessly with the decor.
Environment-Specific Needs
Consider environmental factors like moisture, chemicals, or temperature extremes, especially in industrial settings. Materials like rubber or coated metal are ideal for these conditions.
Determining the Right Size and Quantity
First, measure the width of your cable bundle. Opt for clamps that slightly exceed this measurement for a secure fit. For optimal cable and wire management, evenly space the clips or clamps along the cable path for consistent support and stability.
How to Install Cable Clips on Walls?
Installing cable clips on walls is a straightforward process that enhances cable management for a cleaner, more organised space. Here are the key steps:
1. Preparation
Identify the Cable Path: For wall-mounted TV cable management, plan the route your cables will take. This ensures a neat appearance and functional setup.
Choose the Right Clips: Select electrical cable clamps or clips based on the type and number of cables you need to manage. Additionally, consider the wall material.
2. Marking the Wall
Spacing: Mark the points on the wall where each clip will be placed. For a secure hold, space the clips evenly along the cable path.
Alignment: Use a level to ensure your markings are straight, especially for visible areas in TV setups.
3. Installation
Adhesive Clips: Clean the wall surface before applying. Press firmly for a few seconds to ensure a strong bond.
Nail-In or Screw-In Clips: If using these, pre-drill a small pilot hole to prevent the wall material from cracking. Gently hammer or screw the clips into place.
4. Securing the Cables
Carefully place your cables into the clips or clamps, ensuring they are not overly tightened or pinched, which could damage the wires.
Common Mistakes to Avoid
- Overcrowding: Don't force too many cables into a single clip, as this can lead to damage and reduce the effectiveness of cable management.
- Misalignment: Ensure that all cable holder clips are aligned both horizontally and vertically for a neat appearance.
- Inadequate Spacing: Too much space between clips can lead to sagging cables, while too little can cause undue stress on the wires.
By following these steps and paying attention to the details, you can effectively manage cables on walls, ensuring a neat, safe, and functional space or home office setup.
Can Cable Clips and Clamps Be Used for More Than Just Cables?
Cable clips and clamps are more than mere wire organisers. In Australia, where gardening is a popular hobby and growing industry, these tools become indispensable in maintaining orderly gardens. They can help secure plants, which helps guide their upward growth.
Additionally, their versatility is showcased in various DIY projects and home organisation tasks, such as sturdy support for hanging decorations like festive lights or framed work, demonstrating their wide-ranging applicability and creative potential.
Safety Considerations When Using Cable Clips and Clamps
Follow these safety solutions for managing cables and wires to ensure a hazard-free environment.
- Ensure clips and clamps are rated for the specific cable type and weight to prevent slippage, dislodgement, or structural failure under load.
- Avoid over-tightening, which can damage cables and potentially cause electrical shorts, signal interference, or even breakage of the cable insulation.
- Check for electrical safety, especially when dealing with power cables.
- Regularly inspect for wear and tear to prevent accidents.
- Use insulated clips in areas with high moisture or electrical risks.
- To keep cables out of reach of children and pets, consider routing them higher on walls or behind furniture. Alternatively, you can use cable covers to conceal and secure the wires.
Elevate Your Cable Management Strategy with RS Australia

Transform your space with RS Australia's cable clips and clamps, the ultimate solution for efficient cable management. Delve into our diverse range, where ease of installation meets unparalleled organisation for home, office, and industrial settings. Beyond clips and clamps, we offer various options, including cabletrays, cablesleeves, cable ties, and more, ensuring comprehensive and stylish cable management for any environment.
Popular Cable Clips and Clamps Brands
HellermannTyton
HellermannTyton specialises in safe cable management solutions, crafting innovative cable clips and clamps to support every phase of cable laying and usage across various industries.
Schneider Electric
Schneider Electric designs high-quality cable clips and clamps that align with its goal to support orderly energy optimisation for home and industrial applications.