- Published 21 Mar 2024
- Last Modified 21 Mar 2024
- 5 min
Enhancing Train Operations in Australia: DC Contactors and Relays
Meet the needs of the railway industry with DC contactors, thermal overload protectors, and more. Explore RS's range of quality contactors and relays.

Australia's railway network, one of the most extensive globally, spans over 33,000 kilometres, playing a crucial role in connecting communities and powering the economy. At the core of this network's safety, reliability, and efficiency are essential electrical components. Among these, contactors and contactor relays play pivotal roles, especially in the context of Australian trains and the broader railway industry.
Their significance cannot be overstated, as they are integral to controlling and managing the high-power circuits that are fundamental to trains in Australia and around the globe.

The Basics of Contactors and Contactor Relays
Contactors are electrically-controlled switches used for switching an electrical power circuit, similar to a relay but with higher current ratings. A contactor relay, on the other hand, is a device that operates in response to the electrical output from a control circuit, often used to manage the switching of a larger load or an electrical contactor.
In railway systems, contactors and contactor relays are instrumental in managing and directing the flow of power across a wide array of applications essential to the functionality and safety of trains in Australia. They ensure the smooth flow of power to critical systems, including propulsion, lighting, and heating, as well as the operation of signalling and communication systems. They are designed to handle the rugged demands of the railway environment, including vibration, temperature extremes, and electrical noise.
What is the Difference Between Relays and Contactors?
The main difference between relays and contactors lies in their intended use. Relays are typically used in low power applications for signalling and control purposes, whereas contactors are designed to switch higher power loads.
Contactors are also physically larger than relays due to the need to interrupt larger currents and often include features like thermal overload protection to safeguard against excessive current.
- Application in Circuits: Relays are often used in control circuits and for low power applications, while contactors are utilised for high power applications, such as in the main power circuits of trains.
- Load Handling Capabilities: Contactors can handle significantly larger loads compared to relays. This is crucial in railway operations where controlling large electric motors and other heavy electrical loads is necessary.
- Physical Construction: Contactors generally have more robust construction to deal with the higher power requirements, including arc suppression techniques and larger contacts.
Types of Contactors and Contactor Relays in Railways
In the railway industry, there are several types of contactors and contactor relays, each suited to specific applications.
- DC Contactors: DC contactors are specifically designed for controlling direct current (DC) power systems, which are prevalent in railway applications. These contactors are instrumental in managing the power flow to the propulsion systems of electric trains, where precise control of DC power is necessary for the acceleration, cruising, and braking of trains.
- Thermal Overload Relays: Thermal overload relays are a type of protective device used to safeguard electrical circuits and motors from damage due to excessive heat generated by overcurrents or overload conditions. These relays are critical in preventing overheating by switching off the heating circuit, which can lead to equipment failure, downtime, and even hazardous situations.
Key Roles and Applications
Contactors and contactor relays are fundamental to the smooth operation and safety of railway systems, serving key roles in power management and communication:
- Power Control and Distribution: Contactors and contactor relays are essential for managing high-power circuits within trains, ensuring a smooth and uninterrupted power supply to all systems. They play a critical role in the distribution of power, making them indispensable for the reliability of railway operations.
- Signalling and Communication Systems: These components are also vital in the operation of signalling and communication systems, ensuring trains operate safely and efficiently. Their role in signal control and the integrity of communication networks cannot be understated, as they contribute directly to the safety and coordination of train movements.
Maintenance and Servicing of Contactors and Relays
The Office of the National Rail Safety Regulator (ONRSR), under the Rail Safety National Law (South Australia) Act 2012, plays a crucial role in overseeing and enforcing safety standards within the Australian railway industry. This regulatory framework emphasises the importance of maintenance and servicing of critical electrical components such as contactors and relays, which are essential for the smooth functioning of railway systems.
Regular inspections, testing, and cleaning are essential practices to maintain their performance and reliability. Understanding common issues such as contact wear, coil failure, and improper operation due to environmental factors is vital for timely troubleshooting and repair, ensuring the continuous, safe operation of railway systems.

Partner with RS for Premium Contactors and Relay Solutions
When it comes to enhancing the efficiency and reliability of your train operations in Australia, partnering with RS offers access to a premium selection of DC power contactors and contactor overload relays. RS is committed to providing high-quality solutions that meet the demanding needs of the railway industry.
With an extensive range of products from leading brands, RS ensures that you have the right components to optimise your systems. Whether you're looking for durability, precision, or innovative features, RS's portfolio of contactors and relays is curated to support your operations' safety, efficiency, and reliability
Popular Brands for Contactors and Relay
Siemens
Siemens offers a comprehensive range of contactors and relays that are engineered for precision and reliability. Their products are designed to cater to a wide array of applications within the railway industry, ensuring efficient power management and signal control in challenging environments.
Schneider Electric
Schneider Electric's contactors and relays are renowned for their innovative designs and superior performance. These components are tailored to meet the stringent requirements of the railway sector, offering enhanced safety and operational efficiency.