- Published 27 Feb 2024
- Last Modified 26 Aug 2026
- 13 min
Cat 7 Cable Guide: Specs, Types & Uses
Learn how the Cat 7 cable delivers higher speeds and stronger shielding than its predecessors, and why it remains one of the top choices for demanding network installations across commercial and industrial sectors in Australia.

In this guide, we cover the key specifications, shielding types, and applications of Cat7 cable, and how it compares to Cat 6 and Cat 8 Ethernet standards. Demand for faster, more reliable data transfer continues to grow across commercial and industrial sectors in Australia. Whether you are specifying Cat7 network cable for a new installation or assessing whether Cat7 ethernet cable is the right choice for an upgrade, the sections below cover everything you need to make an informed decision.
What Is Cat7 Cable?

Category 7 cable, more commonly known as a Cat7 or Cat-7 cable, is a type of high-end data transfer patch cable used in delivering the core infrastructure of wired Gigabit Ethernet setups.
Category 7 cable, also written as Cat7 or Cat-7, is a shielded twisted pair network cable designed for high-speed Gigabit Ethernet infrastructure. Classified under the ISO/IEC 11801 Class F standard, Cat7 cabling supports data transfer rates of 10 Gbps over 100 metres of copper at bandwidths up to 600 MHz.ielded twisted pair cable, used principally in achieving high-speed Ethernet connections at data transfer rates of 1 Gbps or higher between directly linked servers, switches and computer networks.
Today, a highly diverse range of commercial and industrial sectors are showing increased demand for faster internet and data transfer speeds - a modern reflection of the fact that we’re continually finding ways to capitalise on the hyper-efficient capabilities of our cutting edge technology. Especially as we move ever closer to a true ‘Internet of Things’ era, where almost any device you can imagine is able to record and transmit potentially valuable user data in real-time, it’s becoming more and more important to stay ahead of an ever-steepening tech curve.
One way in which many users can aim to do just that is to buy Cat7-rated network communication cable when putting together a high-speed internet set up in the workplace or at home. As part of a coherent and comprehensive Ethernet delivery infrastructure, Category 7 cabling represents a valuable step along the path towards optimal speed and efficiency in our wired online experience.
Cat7 Cable Specifications
Cat7 cable specifications are defined under ISO/IEC 11801:2002, classified as the Class F standard. To meet this specification, a Cat7 ethernet cable must satisfy the following performance and construction requirements:
- Deliver reliable data transfer at 10 Gbps over cable runs of up to 100 metres of copper wire
- Support signal frequencies (bandwidth) of up to 600 MHz over the full 100-metre run
- Incorporate four individually shielded twisted copper pairs, plus an overall outer cable shield, to meet the Class F standard's crosstalk and electromagnetic interference (EMI) rejection criteria
- Withstand a defined range of environmental conditions, including temperature variation, mechanical stress, and chemical exposure, without signal degradation
- Be guaranteed for a minimum operational lifespan in continuous use
These requirements position Cat7 cable as a reliable choice for high-density network environments where sustained throughput and signal integrity are both priorities across the full cable run.

Cat7 cable speed
Cat7 was designed to support 10 Gbps Ethernet, although laboratory tests have successfully shown its ability to far exceed this, transmitting up to 40 Gbps at 50 meters and even 100 Gbps at 15 meters - however, precise setups of compatible hardware will likely be needed to achieve these speeds in practice.
To achieve proper Cat7 Ethernet cable speeds specification, cabling runs must be able to support frequencies (bandwidth) of up to 600 MHz over 100m of copper wire. In terms of raw performance versus earlier revisions, this is theoretically 6 times greater than Cat5e (100 MHz), and 2.4 times greater than Cat6 (250 MHz), but we’ll take a slightly deeper dive into the exact differences between all these popular standards in a moment.
Cat7 Cable Standards
Cat7 cabling standards were ratified in 2002 to support 10 Gigabit Ethernet over 100 metres of copper. The cable construction features four individually shielded twisted copper pairs enclosed within an overall outer cable shield, meeting the Class F standard's requirements for signal loss, crosstalk rejection, and EMI resistance over distance.
Cat7 is backward compatible with Cat 5 (Class D) and Cat 6 (Class E) systems, allowing deployment into existing network infrastructure without requiring full replacement of earlier-generation components.
Cat7 Cable vs Other Ethernet Types
What Is the Difference Between Cat6 and Cat7 Cable?
Cat7 cable shares the same four-pair twisted design as Cat 6, and both support 10 Gbps Ethernet over runs up to 100 metres. The key physical distinction is shielding: Cat7 cable applies individual foil screening to each twisted pair as well as an overall outer cable shield as a baseline requirement, providing stronger protection against crosstalk and EMI than a standard Cat 6 cable. Double-shielded Cat 6 variants exist, but dual shielding is built into the Cat7 specification rather than an optional upgrade.
Performance lifespan criteria for Cat7 cable are also more stringent. Selecting between the two for a faster option comes down to installation environment, interference conditions, and budget.
What Is the Difference Between Cat5 and Cat7 Cable?
As noted above, the jump in potential bandwidth performance between Cat 5 and Cat7 Ethernet cable is approximately 6x: Cat 5 supports frequencies up to 100 MHz, while Cat7 cable extends this to 600 MHz. This will, of course, depend to a large extent on other factors, particularly for many home users still connecting via Cat 5 cabling in their Ethernet and LAN setups due in part to its easy installation and routing.
Key considerations here will generally include the capabilities of individual hardware components elsewhere in the system, and the rated speeds available through the internet service provider. Cat7 cable is physically thicker and stiffer than Cat 5, which may affect routing in tight spaces or through existing conduit.
What Is the Difference Between Cat7 and Cat8 Cable?
The Cat8 cable was ratified as a standalone standard under ANSI/TIA 568-C.2-1 and is defined up to 2000 MHz, supporting data transfer rates of 25 Gbps or 40 Gbps depending on the specification tier. However, Cat 8 is designed for short cable runs only, with a maximum distance of approximately 30 metres, making it suited almost exclusively to high-density, short-reach data centre applications.
In terms of Cat7 vs Cat 8 networking performance, Cat7 ethernet cable remains the more practical choice for standard commercial, industrial, and longer-run network installations where 10 Gbps performance over distances up to 100 metres is the core requirement.
Types of Cat7 Cable
Cat7a Cable
The Cat7a specification refers to Category 7 Augmented, introduced under ISO 11801 Edition 2 Amendment 2 (2010) and defined at frequencies up to 1000 MHz. This was likely originally introduced as a future-proofing step for the anticipated wider uptake of a 40 Gbps Ethernet standard; however, in 2016 a new ratification handed this responsibility to Cat 8, specified to 2000 MHz.
Cat7a cable is physically thicker than standard Cat7 due to increased shielding designed to support 1000 MHz performance. Cat7a is not recognised as a wholly separate standard by the US Telecommunications Industry Association (TIA) and sees limited independent equipment support. For most applications, both Cat7 and Cat7a cable types perform similarly, with Cat7a considered appropriate for the most demanding high-density installations.

Cat7 RJ45 Cable
Most pre-packaged Cat7 cable assemblies are terminated with RJ45 connectors at each end, providing immediate plug-and-play compatibility with standard routers, switches, and LAN ports. The RJ45 Cat7 connector is the universal interface for Ethernet connectivity, accepted by virtually all networking hardware regardless of the cable generation in use.
When bulk buying Ethernet cable, though, with Cat7 RJ45 connectors installed. In this case, they’ll need to be bought and wired in as separate components once the networking cable has been cut to the desired run length and routed appropriately. In this scenario, two wiring schemes (T568A and T568B) are used to terminate the ends of the twisted copper pairs found inside the jacketing of a Cat7 cable onto the RJ45 connector interface.
When purchasing bulk Cat7 cable for custom-length runs, the cable arrives unterminated and Cat7 connector ends must be wired in separately once the cable has been cut and routed to the required lengths. Two wiring schemes are used to terminate the twisted copper pairs onto the RJ45 interface:
- T568A, common in residential and government installations across Australia
- T568B, the standard for most commercial and industrial networks.
Either scheme is compatible with Cat7 cabling, provided both ends of each cable run are terminated consistently using the same scheme.
What Does UTP, FTP, SFTP, STP and SSTP Mean?
Whether you are assessing Cat7 cable options for an upgrade, or specifying bulk Cat7 cabling for a major network installation, you will often encounter acronyms such as UTP, FTP, and SFTP in manufacturer and supplier product listings.
These prefixes describe the shielding configuration inside the cable body and can affect weight, flexibility, cost, and EMI performance.
UTP Cat7 Cable
Cat7 UTP (Unshielded Twisted Pair) cable denotes an Unshielded Twisted Pair design. In this configuration, the four pairs of twisted copper wires inside a Cat7 cable are sheathed only by their own interior jacketing and that of the external cable.
UTP Cat7 cable is typically the most cost-effective variant, providing adequate EMI and signal attenuation protection to meet the baseline Cat7 specification.
F/UTP Cat7 Cable
F/UTP Cat7 cabling retains unshielded individual pairs but adds a single foil screen encasing all four pairs collectively beneath the outer jacket. The Foiled/Unshielded Twisted Pair configuration provides a moderate improvement in signal protection above the UTP baseline, reducing susceptibility to external interference without the added weight of individually shielded pairs.
STP Cat7 Cable and FTP Cat7 Cable
Where you see Cat7 cable labelled as either STP or FTP, these acronyms stand for Shielded Twisted Pair or Foiled Twisted Pair respectively and essentially mean the same thing. Both STP and FTP Cat7 cabling feature an additional layer of protective foil screening wrapped around each individual pair of twisted wires inside the cable, providing stronger per-pair interference rejection than F/UTP.
SFTP Cat7 Cable and SSTP Cat7 Cable
The most comprehensive level of additional signal protection for Cat7 cable is typically provided by SFTP (Shielded Foiled Twisted Pair) or SSTP (Shielded Screened Twisted Pair) configurations. Both combine an outer foil screen encasing the inner conductors and individual foil wrapping around each twisted pair, providing the highest level of EMI protection available in the Cat7 cabling range and making them the preferred choice for high-interference industrial environments and densely cabled data centre installations.
What Is a Cat7 Cable Used For?

Using ethernet cables at Cat7 specification provides a reliable path to 10 Gbps performance with strong noise immunity across a range of demanding environments. Cat7 and Cat7a cabling is used across commercial, industrial, and residential networks wherever high-speed, interference-resistant connectivity is required.
Cat7 Ethernet cables
Category 7 Ethernet cables (also referred to as Cat7 LAN cables in everyday use) are used to form the connective tissue between modems, hubs and individual computers on networks of all shapes and sizes. These can range from sprawling data centres and server environments, through to individual home setups where enthusiasts seeking higher speeds and lower latencies turn to Cat7 cable for gaming, streaming and up/download performance boosts.
Commercial and industrial uses for Cat7 cable
Cat7 cables were originally developed for use in larger-scale industrial Ethernet networks - and, as such, they’re designed not only to provide high speeds and bandwidth capabilities, but also to withstand a broad range of environmental and mechanical hazards.
This can include anything from temperature extremes and UV/moisture exposure, to direct contact with a wide range of solvents, oils and chemicals, making Cat7 wire an equally ideal choice for robust outdoor applications such as railway cables.
Domestic uses for Cat7 cable
In addition to enthusiast gaming setups, Cat7 cables have become increasingly popular with home users across a wide range of domestic LAN cable networks and connectivity setups in recent years.
While it’s certainly true that very few typical home hardware setups will support anything like the sorts of data transfer speeds and bandwidths that Cat7(a) Ethernet cabling can, using the highest revision wire you can will still offer potential performance boosts in many basic router-to-device networking scenarios.
Additionally, many people first bought into Ethernet connectivity fairly early on in the home hub era (around the Cat5 cable revision or earlier), and naturally look to the latest versions when needing to replace or upgrade older cables. Those planning to wire a smart home today, for example, might typically gravitate towards Cat7 and Cat7a as a future-proofing measure, anticipating the continued acceleration of home hardware and connection speeds over the coming years.
One thing to bear in mind when upgrading or replacing a home network cabling setup is that Cat7 and Cat7a versions tend to be considerably thicker, stiffer and heavier than their Cat5 predecessors, and this may affect on your ability to route the cables neatly in places where space is at a premium or very precise bends are required.
How to Choose a Cat7 Cable
Choosing the rightcable for a Cat7 installation depends on the physical environment, the run length, and the level of interference protection the network demands. The following factors guide most Cat7 cabling selection decisions:
Installation Type
Fixed installations in conduit or trunking suit standard Cat7 cable with a rigid construction and static sheath. Flexible or drag-chain deployments, common in industrial machinery and robotic systems, require cables specified for repeated movement, with a flexible sheath and individually screened pairs that maintain integrity under sustained mechanical stress.
Cable Run Length
Cat7 network cable supports 10 Gbps over runs up to 100 metres. Runs beyond this distance require active components such as managed switches or signal repeaters to maintain throughput and signal integrity across the extended span.
Shielding Requirement
Low-interference environments such as standard office networks are adequately served by UTP or F/UTP Cat7 cabling. High-EMI environments, including industrial facilities with heavy switching equipment, variable-speed drives, and motor systems, require S/FTP or SSTP configurations for reliable signal performance.
Sheath Material
PVC sheathing suits standard indoor installations. PUR (polyurethane) sheathing is preferred for harsh or industrial environments subject to mechanical wear, oils, or solvents. LSZH (Low Smoke Zero Halogen) sheathing is specified for confined spaces, tunnels, and applications where fire safety and toxic smoke emission are a concern.
Summary
When planning or shopping for the right type of Ethernet networking cables for your needs, it’s important to remember that there are numerous grades, distinctions and categorisations even within a particular version/revision of Ethernet cabling.
For Cat7(a) cables, you can optimally support current and future network speed potential by selecting products that benefit from more advanced additional shielding, or by designing the network such that distances are reduced and signal attenuation is minimised. In many applications, these sorts or variables can often give dramatically different results, even for two setups using functionally identical Category 7 or Cat7a cables.
Frequently Asked Questions About Cat7 Cables
Related links
- RS PRO Black Low Smoke Zero Halogen Sheath, U/FTP
- RS PRO Yellow, Shielded Low Smoke Zero Halogen Sheath
- RS PRO Black Polyvinyl Chloride Sheath, SF/FTP
- Ethernet Cable
- Van Damme TourCat Cat 7 Shielded, Black Screened Polyurethane Sheath
- Cat5 Vs Cat6 Ethernet Cables and What You Need to Know
- KabeltronikCAT 7 Mobil HighFlex STP -C Black, S/FTP PVC Sheath
- RS PRO Black Polyvinyl Chloride Sheath, U/FTP