- Published 8 Mar 2024
- Last Modified 8 Mar 2024
- 6 min
A Complete Guide to Electrical Tapes for Home DIY Projects
With the rise of home DIY projects, learn about the different types of electrical tapes used for various applications, from home improvement to repairs.

Many homeowners in Australia today partake in home DIY projects, with 57% of them considering themselves “DIYers.” According to a survey by Newgate Research, 46% of DIYers are motivated to do their own DIY home project to make their houses more appealing and comfortable. Moreover, 44% think that it is more affordable compared to hiring someone else to do the job for them.
With the rise of DIY home improvement projects in the country, it’s essential to be well-versed in the various equipment, including a handy electrical tape.
Electrical tapes can be used for various applications, from home repairs to crafty DIY projects. There are many types of electrical tapes available in the market today, and with this, we give you all you need to know about them and how they are used.

Choose the Right Electrical Tape for Specific Applications
With electrical tapes, one size certainly does not fit all. These tapes are crafted from various materials, each with unique properties tailored to specific needs and applications. Here are some of the common types of electrical tapes and their applications:
1. Vinyl Electrical Tape
Vinyl electrical tapes are your go-to option if you want a versatile and durable electrical tape for various applications. Its flexible nature allows for easy application around irregular shapes and tight spaces, making it a staple in various DIY projects. Whether insulating wires, bundling cables, or marking circuits, vinyl tape offers reliable performance and long-lasting adhesion. This type of electrical tape is also waterproof, making it great for indoor and outdoor applications.
2. PVC Electrical Tape
Another essential type of electrical tape to consider is PVC electrical tape. PVC tape is known for its excellent insulation properties and can be used for various electrical applications. It provides reliable protection against moisture, chemicals, and abrasions, ensuring the longevity and safety of your electrical installations. PVC tape is also flexible and easy to work with, making it ideal for professional and DIY projects.
Rubber Electrical Tape
When it comes to sealing and insulating electrical connections, rubber electrical tape can be a great choice. Renowned for its exceptional elasticity and adhesion properties, rubber tape forms a strong, reliable seal that withstands the test of time. Whether you're repairing frayed wires, splicing cables, or securing connectors, rubber tape provides an extra layer of protection against moisture, chemicals, and abrasions. It can conform to irregular surfaces, preventing potential hazards and ensuring the safety of your electrical installations.
4. Polyimide Film Tape
For applications that require heat-resistant electrical tape, polyimide film tape emerges as the ultimate solution. This specialised tape can withstand temperatures ranging from sub-zero to scorching hot, making it indispensable in the electronics, automotive, and aerospace industries. Whether you're soldering circuit boards, insulating high-temperature wires, or protecting sensitive components, polyimide tape offers unparalleled thermal stability and reliability. Its non-conductive properties prevent short circuits and electrical failures, providing critical insulation in demanding environments.
Safe and Effective Use of Electrical Tapes in Repairs
Safety should always be a top priority when handling electrical repairs at home. Follow these step-by-step guidelines to ensure the safe and effective use of electrical tapes:
1. Prepare the Surface
Before applying electrical tape, it's crucial to prepare the surface properly. This entails ensuring that the area is clean, dry, and free of any debris or grease. Any contaminants on the surface can affect the tape's adhesion and lead to poor insulation or potential hazards. By taking the time to clean and prepare the surface, you can ensure optimal adhesion and longevity of the repair.
2. Proper Insulation
Insulation is the cornerstone of electrical tape usage in repairs, especially when dealing with exposed wires or connections. Proper insulation not only protects against electrical shocks but also prevents short circuits and potential fire hazards. When applying the right electrical insulation tape, ensure that all exposed wires or connections are thoroughly covered to create a secure barrier. Pay close attention to overlapping layers to ensure uniform coverage and effective insulation.
3. Adhere to Australian Safety Standards
Adhering to Australian safety standards and regulations is non-negotiable when performing electrical repairs at home. Make sure that when you do wiring repairs using electrical tape, it adheres to the standards under AS 2067 and AS/NZS 7000. The AS 2067 refers to the standards set for substations and high voltage installations exceeding 1 kV a.c. On the other hand, AS/NZS 7000 is the overhead line design of the electrical wires. If you're unsure about any aspect of the repair process, don't hesitate to seek assistance from a qualified electrician. Know that your safety should always be the top priority.
4. Handling Environmental Factors
Australia's unique environmental factors, such as extreme heat and humidity, can impact the performance of electrical tapes over time. Therefore, it's essential to choose tapes that are specifically designed to withstand these conditions for reliable insulation and long-term durability. Look for tapes that are labelled heat-resistant and waterproof, as they offer enhanced protection against moisture ingress and temperature fluctuations. By selecting tapes tailored to the Australian climate, you can ensure that your repairs remain secure and effective, regardless of environmental challenges.

Creative and Practical DIY Crafts with Electrical Tape
Beyond repairs, electrical tapes offer endless possibilities for creative DIY projects around the home. Here are some ideas to spark your imagination:
- Wall Decor: For your next home DIY project, use coloured electrical tapes to create eye-catching patterns or designs on walls, adding a unique touch to your home decor.
- Personalisation: Customise household items like laptops, phone cases, or storage containers by embellishing them with coloured electrical tape.
- Craft Projects: Get crafty with electrical tape by incorporating it into projects like homemade greeting cards, gift wrapping, or even fashion accessories.
Find Electrical Tapes for a Wide Range of Applications at RS Australia
When it comes to sourcing electrical tapes for your home DIY projects, RS Australia has you covered. Our extensive range of products caters to diverse needs, ensuring you'll find what you need to complete your projects with confidence. From adhesives to electrical wires, we offer a comprehensive selection of tools and equipment from trusted brands.
Conveniently browse and order online to access high-quality products that meet your requirements and exceed your expectations. For more insight into handy adhesives, learn about the different types of gaffer tapes.
Recommended Electrical Tape Brands
Hellermann Tyton
Renowned for its commitment to excellence, Hellermann Tyton delivers high-quality electrical tapes designed to meet the demands of modern industries. Their tapes offer excellent adhesion and resistance to environmental factors, ensuring long-lasting performance in challenging conditions.
Advance Tapes
With a reputation for excellence and innovation, Advance Tapes offers a comprehensive range of electrical tapes tailored to specific needs. From heat-resistant tapes to waterproof varieties, Advance Tapes provides reliable solutions for diverse applications, making them one of the preferred choices among professionals and DIY enthusiasts alike.