A Complete Guide to MCBs

What are MCBs and how do they work? Discover all you need to know in our comprehensive guide.

MCBs Banner

This guide to miniature circuit breakers (MCBs) explains everything you need to know about the types and sizes available. We outline the best brands and explain the function of MCBs in your electrical projects.

What is an MCB?

Let’s start with the basics – just what is a miniature circuit breaker? An MCB is an automatically operated electrical switch. Miniature circuit breakers are intended to prevent damage to an electrical circuit as a result of excess current. They are designed to trip during an overload or short circuit to protect against electrical faults and equipment failure.

MCBs are widely used as isolating components in domestic, commercial, and industrial settings. They form part of a broader family of more powerful circuit-breaking components.

MCB Labelled Diagram

How Does a Miniature Circuit Breaker Work?

Mini circuit breakers are triggered by overcurrent - electrical current that exceeds a designated safe current and makes use of a relatively robust mechanical mechanism designed to minimise failures and false alarms.

Excess current causes the bimetallic strip within the MCB to heat, bend, and trip. This releases a switch which moves the electrical contact points apart to confine the arc (electrical discharge). The arc is divided and cooled by an insulated metal strip called the arc chute. The contacts close again once the fault has been fixed and the MCBs are reset.

An MCB is designed to protect against both overloading and short-circuiting. These are detected differently using separate processes. Overload protection is provided by the bimetallic strip using thermal operation, whereas short-circuit protection is provided by the tripping coil via electro-magnetic operation.

If the discharge is especially high, the MCB will trip (activate) very quickly – within one-tenth of a second. When the overcurrent is closer to the safety limits, the component will be slower to respond.

Different MCB Types Explained

Several different MCB types are available – types A, B, C, D, K, and Z. However, the three key versions are type B, type C, and type D. Each is designed to be responsive to the likely strength of electrical surges in different settings. These variations are typically known as their ‘trip curve’ but can also be known as their tripping characteristics or overcurrent characteristics.

Let’s take a look at the differences between each primary type:

Type B MCBs

Type B MCB

Type B circuit breakers are designed to trip if the current flowing through hits between three and five times the recommended maximum or ‘rated load’.

This is the most sensitive type of MCB, designed for domestic applications, and low voltage commercial settings where any current surges are likely to be small.

Browse Type B MCBs

Type C MCBs

Type C MCB

Type C circuit breakers are used for more powerful electrical devices where any surges are likely to be higher – typically commercial and industrial environments.

They are designed to trip at currents between five and ten times their rated load. Good examples include smaller electric motors and fluorescent lighting.

Browse Type C MCBs

Type D MCBs

Type D MCB

D-type MCBs are the least sensitive type, only activating when current surges to between ten and twenty times the recommended maximum.

D-rated MCBs are built for heavy-duty commercial and industrial devices where very strong current surges occasionally occur. Examples include welding equipment, X-ray machines, large motors, and uninterruptible power supply units.

Browse Type D MCBs

Other MCB Types

A few more specialised MCB models are available. These include:

  • Type K MCBs – these will trip when current reaches eight to twelve times the recommended maximum. They are a good choice for motors

  • Z-type MCBs – these are highly sensitive MCBs, tripping when current exceeds the rated load by only two to three times. They are used with more delicate devices prone to short circuits, such as semiconductors

How to Choose the Right MCB

The type of MCB that you should buy depends on the specifics of your device or installation. When shopping for an MCB, compare the following factors:

  • The tripping characteristics

  • The breaking capacity – the maximum current a circuit breaker can interrupt without destruction or releasing an arc. This needs to match the likely strength of any surges in the vicinity of the installation. Breaking capacities are measured in kiloamperes (kA), each of which is 1,000 amperes (amps), the standard unit of electrical current

  • The number of poles or trippable switches within the MCB housing. Pole options include single, double, triple and neutral, and four-pole. Triple or three-pole models are common; these can simultaneously break the current on all three circuits if a fault occurs on any one

Single Pole

Single Pole MCBs

Double Pole

Double Pole MCBs

Four-Pole

Four-Pole MCBs

MCB Choices by Ampere Rating

The following lists some of the most frequently-encountered load capacities for commercial MCBs:

MCB Choices by Breaking Capacity

The following are the most frequently-encountered breaking capacities of commercial MCBs:

4.5kA

4.5kA MCBs

5kA MCBs

5kA MCBs

6kA MCBs

6kA MCBs

 

MCBs by Brand

Key MCB brands are compared in the following chart:

Image Brand & Product Type Main Benefits Typical Applications
ABB MCBs Complete range of MCBs to cover most applications

Space and time-saving design
Residential, commercial and industrial applications
Eaton MCBs Professional range of MCBs

Safe and reliable
Commercial and industrial
Legrand MCBs Leading-edge technical features

High-performance ranges
Residential, commercial and industrial applications
Schneider MCBs Excellent circuit protection

Rigorously tested
Wide range of applications; industrial and commercial
Siemens MCBs High-performance range

Innovative mounting options
Wide range of applications
Europa MCBs Perfect for consumer unit fitting

Fully tested and conform to all relevant standards
Perfect for residential applications

FAQs

How Do You Test MCBs?

To test an MCB after installation, you will need a suitable portable voltage meter from a reputable manufacturer. Electricians also recommend manually inspecting the switching mechanism of MCBs before installation; typically, a greater degree of pressure is needed to open and close more reliable models.

Can You Mix MCBs?

Specifications matter more than brand when choosing MCBs, so in theory, you can use any component that is compatible with a particular device. However, mixing brands in the same installation is not recommended as it makes testing less reliable and can invalidate warranties and installation guarantees.

Why are MCBs Preferred to Fuses?

MCBs serve a similar function to electrical fuses, which are designed to melt and thereby break a circuit if the current flowing through exceeds a designated limit. However, fuses can be less reliable than MCBs - the latter work better in lower voltage settings and do not require replacement after use.

What is the Difference Between MCBs and MCCBs?

Moulded case circuit breakers (MCCBs) have a very similar function to MCBs but they also have a higher capacity. MCBs are all sub-100-amp devices and are designed for low voltage circuits, so their trip curves cannot be adjusted. By contrast, MCCBs feature adjustable trip characteristics, which means that they can be used with higher voltages – as much as 2,500 in some instances.

What is the Difference Between MCBs and ELCBs?

ELCBs (earth-leaking circuit breakers) use earthing as their primary method of controlling electrical current and preventing electrocution. They work by detecting any stray voltage on the enclosure of a device and then breaking the circuit if it exceeds a designated level. They perform a similar function to RCDs, but the latter detect stray voltage directly and so are now more favoured by electricians.

What is the Difference Between MCBs and RCDs?

Residual current devices (RCDs) are a different form of electrical safety equipment. While MCBs have a general function, RCDs are specifically built to protect against the frequently fatal risk of electrocution from touching exposed wires or incorrectly earthed cables. They operate directly within electrical circuits to detect faults and cut off potentially hazardous currents.

RCDs are also available in various different types – types A, B, C, D, K, and Z. In the United States and Canada, they are known as ground fault circuit interrupters (GFCIs).