Everything You Need To Know About Socket Screws
![socket-screw-guide-banner-img](https://uk.rs-online.com/euro/img/general/task-request/20256/socketscrews_980x180px.jpg)
In this guide, we’ll cover some of the various different socket screw types, materials and designs currently sold on the worldwide market, and discuss which sorts of socket set screws are best to use across a range of specific applications or mounting requirements.
What is a socket screw?
Socket screws are a variant on traditional screw formats that are designed and manufactured with a hexagonal (hex) internal drive built into the head. As such, they’re intended to be tightened and loosened with an Allen wrench or hex key, as opposed to a traditional screwdriver.This is really the key feature that sets a socket screw apart from many other, arguably more familiar screw head drive styles - products such as the classic cross/Phillips head screw, the universal slotted/flathead version, and the increasingly common Pozidriv (star-shaped) variants.
Another common distinction is that socket screws are often squared off at the tip; these are generally referred to as flat point socket screws, and they tend to be the most widely used type found in many day-to-day applications. Note, however, that various other designs - such as cone point, cup point and dog point socket screws - are also available, as we’ll see further on in this guide.
In most other regards, including such cosmetic details as general size, shape and finish options, there isn’t typically much physical difference between socket screws and regular screws for the majority of everyday uses. So what exactly is the point of a socket screw, and when should you use one?
In short, the design of a socket screw is effectively an attempt to combine some of the increased performance features of other common hex fasteners - nut and bolt systems being the obvious point of reference - with the convenience and ease of use of a standard format screw set. This middle ground can be a useful compromise in many situations, particularly when working in spaces that don’t allow sufficient space or ease of access for securing externally wrenched hex fasteners (again, bolts would be the obvious comparison here).
Advantages of socket screws
The potentially higher torque and clamping force that can be achieved with a socket screw over a regular screw makes them a preferable option in some common use cases. When rated up against regular screws and bolts in a like for like test, socket screws can often deliver some or all of the following advantages in relevant scenarios:- Since socket screws typically offer greater clamping force than standard screws and many other small-format fastener types. This means that fewer socket screws can be used in a given application to achieve the same overall clamping force on the joint or workpiece.
- Using fewer screws means:
- Reduced hardware costs
- Fewer holes to drill and tap into mounting or mating surfaces, saving time and reducing potential damage to components
- Lower overall weight of the finished piece
- The trend towards lightweight constructions when using socket screws is further enhanced due to their smaller individual size than many other screw types and other fastening components - especially compared to nut and bolt fixing arrangements. In particular, the cylindrical heads and internal drives of socket screws are far smaller in diameter than fasteners with external hex heads, and therefore need less space (with no additional room needed to manoeuvre a wrench) for installation
What is a socket head cap screw?
The generic name 'cap screw' was traditionally used as something of an umbrella term, meaning any of various screw types chosen for fastening applications where the use of a nut and bolt installation was deemed unsuitable. However, today it tends to refer specifically to a particular style of screw head.Any number of different screw types and shapes can incorporate elements of the basic cap screw head design - you might find anything from shoulder screws and countersink screws, through to button and fillister head screws, described broadly as 'cap screws'. A socket head cap screw is also commonly referred to as a socket cap screw, Allen bolt, or simply a socket screw (in many ways, it's very much the 'standard' version of a socket screw).
Socket head cap screws are very widely used along all manner of industrial production and assembly lines, including in the automotive sector, cabinetry and furniture manufacture, machine tooling applications and steel fabrication. This is chiefly thanks to the fact that they’re easy to install and tighten/loosen, as well as providing impressive clamping strengths while retaining a discreet and tidy finished look.
As with the vast majority of all socket screws, the socket head cap screw features a cylindrical head with an internal hex drive hole, and is most often (although not always) threaded all the way along the full length of the shank. And, also like nearly all socket screws, they're primarily designed to be used in assemblies where there isn't sufficient clearance to install a conventional nut and bolt, or to manoeuvre a standard socket wrench.
Socket screw sizes
The average socket cap screw head is around 1.5 times the diameter of the screw shank, and about as high as the shank is wide. However, alternative head designs for socket head cap screws include low head, button head and flat head varieties, intended for driving into countersunk holes and other application-specific mounting positions.
When looking to buy socket screws, note that the product’s stated length is typically measured from immediately under the head to the tip. (This is the case for most screw types, but some specific varieties - thumb screws, for example - will often give stated length measurements that include the height of the head in the overall specification.)
Most socket screw types are available in either metric or imperial measurements (or both) for length and diameter, depending on the particular manufacturer or supplier in question. Many leading brands of socket screw manufacturers, will often provide suppliers with a socket screw sizing chart or similar tool that can be referred to at the point of purchase.
While relatively small socket screw sizes (of diameters ranging from M2 to M6, and lengths of around 3mm to 20mm) tend to be more in demand across a wider range of tasks and applications, the full range of available sizes is considerable. Larger, heavier gauge and extra long socket screws are not at all uncommon, particularly in widths of around M8 to M20, and lengths of anywhere up to 130mm.
Extra long socket screws are especially frequent requirements for use in electrical plug sockets. Common electrical socket screw sizes include 40mm, 50mm, 60mm, 75mm and 100mm.
![M4 socket screws RS-PRO-M4-12mm-Hex-Socket-Cap-Screw-Plain-Stainless-Steel-img](https://media.rs-online.com/t_large/F0281035-03.jpg)
M4 socket screws
![M5 socket screws RS-PRO-M5-12mm-Hex-Socket-Cap-Screw-Plain-Stainless-Steel-img](https://media.rs-online.com/t_large/F2328237-01.jpg)
M5 socket screws
![M6 socket screws RS-PRO-M6-12mm-Hex-Socket-Cap-Screw-Plain-Stainless-Steel-img](https://media.rs-online.com/t_large/F2328287-02.jpg)
M6 socket screws
Socket screw materials
There are many different materials used in the manufacture of socket screws, including the very common steel and stainless steel varieties, as well as brass, aluminium, black nickel or zinc-plated and even chrome socket screws. The ideal material to choose will depend entirely on the specific application you’re intending to use the socket cap screw set in.Aluminium Socket Screws
Aluminium socket cap screws are often preferred for applications in which weight is a key consideration - these might include anything from the automotive industry through to domestic uses such as installing hardware and trim on moveable furniture, cabinets, doors and windows.Despite only being around one third the weight, aluminium is durable, but rather less so than steel, and tends to have lower shear strength in particular. While aluminium offers decent performance in terms of corrosion resistance in more challenging environments, it’s less hardwearing in this regard than stainless steel.
Aluminium socket screws are also typically seen as unsuitable for use in most kitchen utensils and food preparation/production line roles. Stainless steel is again preferred here, due to aluminium’s ability to influence the flavours and appearances of certain foodstuffs under the right (wrong?) conditions.
Other socket screw materials are detailed below.
Zinc and/or nickel plated steel socket screws
![RS-PRO-Hex-Socket-Cap-Screw-Zinc-Steel-M5.jpg](https://media.rs-online.com/t_large/F4915243-01.jpg)
The primary reason why so many steel socket cap screw sets are available with zinc, nickel or zinc-nickel plating options is for the superior corrosion (rust) resistance this simple manufacturing process can offer screws of all types.
Combined zinc-nickel plating is generally considered a tougher coating (up to twice the hardness) when compared to standard zinc plating, and can also deliver up to four times the corrosion resistance of other metallic coating processes. However, it’s typically a fair bit more expensive, and may not be considered an especially cost-effective option in many applications where standard galvanised steel socket screws would suffice.
Common industrial uses of zinc-nickel plated socket screws might include:
- Military and aerospace construction
- A wide range of marine and automotive-grade fastening solutions
Brass socket screws
![RS-PRO-M6-30mm-Hex-Screw-Plain-Brass-img](https://media.rs-online.com/t_large/F4832390-01.jpg)
Brass socket cap screws might often be preferred for their aesthetic value, but as an alloy of copper and zinc, brass or brass tipped socket screws may offer certain other advantages in certain situations. Brass is stronger than copper alone, although it will still be considerably less rigid than most varieties of steel or stainless steel socket screws you’ll encounter.
However, note that brass plating will be less resistant to corrosion than solid brass socket screws, and as such you should make sure you know exactly what you’re buying before choosing a product for use in more exposed locations.
Suitable for:
- Outdoor use
Types of socket screws
As well as different materials, socket screws are also available in different types:Button head socket screws
Button head socket cap screws are also known as round head or dome head socket screws. As the name implies, they’re manufactured with a smooth, slightly rounded dome or ‘button’ at the head end, which tends to be somewhat larger and more bulbous than standard cap screw varieties.
Often this means that a button head socket screw can accommodate a larger gauge of hex key or driver, and thus can be affixed with more torque to achieve greater clamping forces. However, smaller sized hex socket button screws should be fastened with less torque.Button socket screws can also be supplied with tamper-proof drives.
The top advantages of button head socket screws are:
- They cannot cause damage to other objectsor materials or injury to passersby because their smoothly domed head has no protruding or sharp angles.
- They are a great choice for realisty light duty tasks.
Flat/countersunk socket screws
![RS-PRO-M6-12mm-Hex-Socket-Countersunk Screw-img](https://media.rs-online.com/t_large/F0171887-01.jpg)
Hex socket countersunk screws, also known as flat or flat head socket screws, are used in applications where it’s vital that the installed screw sits flush with or just below the surface of the workpiece.
Countersunk socket screws feature a sloping shoulder design - usually at a standard angle of around 82 degrees - that allows the screw to bed down into the surface via a pre-drilled countersunk hole. Again, they’re sold in numerous lengths and widths, and are widely available under both imperial and metric socket screw sizing charts.
Suitable uses:
- Furniture-making and home decor projects, where aesthetics are paramount
- Situations where protruding heads may be a safety concern
Top picks
There’s a wide range of types to choose from – browse our top brands by clicking the link to view the full product range.![RS PRO rs-pro-logo](https://media.rs-online.com/brand/M3385-01.jpg)
RS PRO socket screws