• Published 8 May 2025
    • Last Modified 8 May 2025
  • 10 min

How to Choose the Best Thermal Paste & Grease: Thermal Compound Recommendations

Choose the best thermal paste for your CPU/GPU. Guide on conductivity, viscosity, & brands like RS PRO. Expert tips & FAQs.

RS marketing banner

Thermal paste, also known as thermal grease or heat sink compound, is a substance applied between heat-generating components like CPUs and other types of processors and their heat sinks. Its role is to fill the microscopic air gaps that would otherwise create a barrier to efficient heat transfer, thereby ensuring optimal heat dissipation. Effective thermal management is crucial because even slight temperature increases can significantly reduce the lifespan and performance of electronic components.

Choosing the right thermal paste is essential for maintaining optimal operating temperatures, especially in demanding applications like high-performance gaming PCs, intensive workstations, and industrial machinery where thermal stress can lead to system failures.

This guide will provide a clear breakdown of the key considerations when choosing thermal pastes, such as thermal conductivity, viscosity, and compatibility, so you can make an informed decision on the best thermal cooling paste for you.

Key Considerations When Choosing Thermal Paste

Selecting the right thermal compound paste involves evaluating several key factors to ensure optimal performance and compatibility with your specific application. Whether you're building a high-end gaming rig or maintaining industrial equipment, understanding these considerations will help you make an informed decision. For a breakdown of recommended products, jump to "Best Thermal Paste and Thermal Grease", or continue reading for a detailed look at the factors to consider.

  • Thermal Conductivity (W/mK): Measured in Watts per meter-Kelvin (W/mK), thermal conductivity indicates the paste's ability to transfer heat. A higher W/mK rating signifies a greater capacity to conduct heat away from the component, resulting in lower operating temperatures and improved system stability, especially under heavy loads. This is a crucial metric for high-performance applications where efficient cooling is paramount. In industrial settings, where components may operate under continuous stress, a high W/mK rating is essential for maintaining consistent performance. To learn more about electrical measurements, read our blog post on the difference between watts and volts.
  • Viscosity & Application Ease: Viscosity refers to a fluid's resistance to flow. In thermal paste, it dictates how easily the compound spreads across the component's surface. Lower viscosity pastes flow readily, making them simpler to apply and ideal for users who are new to thermal paste application. Higher viscosity pastes, while potentially more challenging to spread evenly, often provide better long-term stability and resistance to pump-out (the gradual displacement of paste due to thermal cycling), making them good options for professionals seeking sustained performance.
  • Curing Time & Longevity: Consider both curing time and longevity when selecting thermal paste. Some pastes offer immediate peak performance, ideal for quick testing, while others require a curing period for stability. Longevity, the paste's effective lifespan, is equally important. Match these characteristics to your application's requirements for optimal results. In mission-critical systems, a long-lasting, stable thermal paste can minimise maintenance and downtime.
  • Electrical Conductivity & Safety: Certain thermal pastes, particularly liquid metal varieties, are electrically conductive, offering superior thermal transfer. However, this conductivity poses a risk of short circuits if not applied meticulously. Consequently, these pastes are best suited for experienced users. For those new to thermal paste application, or in scenarios where safety is a primary concern, non-conductive pastes are the recommended choice.
  • Compatibility with CPU/GPU/Other Components: Ensuring compatibility between your thermal paste and components is paramount. Certain pastes, like liquid metal compounds, can react negatively with specific materials. For instance, aluminium, often used in heat sinks, can corrode when in contact with liquid metal. Standard pastes, formulated with silicone or ceramic, offer wider compatibility. Therefore, reviewing the specifications of both your processors or components and the chosen thermal paste is essential to prevent damage.
  • Price vs. Performance: The cost of thermal compounds can vary significantly. While high-end options promise the best possible thermal performance, it's important to consider if that level of performance is necessary for your application. Many affordable pastes offer excellent heat transfer capabilities and represent a wise investment for most users.

Best Thermal Paste and Thermal Grease

When selecting a thermal paste, choosing reputable brands ensures reliability and performance. Here's a look at some of the top brands available at RS Australia, known for their quality and diverse product ranges:

RS PRO Thermal Grease

RS PRO Thermal Grease

Brand Overview:

  • RS PRO delivers high-quality, industrial-grade thermal grease, rigorously tested for reliability in demanding applications across various industries.They emphasise quality control to ensure consistent performance under challenging conditions.

Product Range:

  • Their range includes non-silicone and metal oxide options, catering to diverse thermal needs, from CPU cooling to specialised industrial heat transfer.

Key Features:

  • RS PRO thermal greases offer consistent performance across wide temperature ranges, ensuring durability and reliability in challenging environments.
  • Their robust formulations are designed to withstand extreme conditions.

Unique Selling Points:

  • They provide a cost-effective balance of performance and versatility for a broad spectrum of industrial applications, making them a practical choice for budget-conscious professionals.

Popular Models:

TheRS PRO Non-Silicone Thermal Grease, 4W/m·K is ideal for Australian environments where silicone contamination is a concern, offering consistent thermal performance in varying climates. This product's non-silicone composition makes it suitable for sensitive applications.

Availability:

  • Readily available for online purchase via the RS Australia site.
Electrolube Thermal Grease

Electrolube Thermal Grease

Brand Overview:

  • Electrolube specialises in innovative electro-chemical solutions and reliable thermal management products.

Product Range:

  • Their selection includes both silicone and non-silicone options, designed to meet various thermal conductivity requirements. This diversity allows for precise matching to specific application needs.

Key Features:

  • Electrolube ensures optimal performance and long-term reliability as well as application-specific formulations for demanding Australian industrial environments.

Unique Selling Points:

  • They provide high thermal conductivity and long lifespan, ideal for demanding, critical applications, minimising maintenance and ensures continuous operation.

Popular Models:

Electrolube Silicone Thermal Grease (0.9W/m·K)is ideal for Australia's diverse climate due to its long-term stability and resistance to environmental factors, making it a popular choice. Its reliable performance is well-suited for a wide range of electronic applications.

Availability:

  • Conveniently available on RS Australia.
Chemtronics Thermal Grease

Chemtronics Thermal Grease

Brand Overview:

  • Chemtronics provides high-quality electronic maintenance and repair products, including thermal management solutions. Their products are designed to meet the rigorous demands of electronics professionals.

Product Range:

  • They offer a range of thermal greases, including non-silicone, boron nitride, and silicone-based options, designed for electronic components and assemblies.

Key Features:

  • They offer easy application and reliable performance in sensitive electronic applications, designed for precision and reliability.

Unique Selling Points:

  • Chemtronics is a go-to choice for high-quality electronic maintenance and repair.

**Popular Models:

**This Boron Nitride Thermal Grease, 1.85W/m·Kis ideal for Australian electronics technicians due to its non-conductive properties, essential for preventing electrical shorts in sensitive electronic equipment

Availability:

  • Readily available through the RS Australia website.
Bergquist Thermal Grease

Bergquist Thermal Grease

Brand Overview:

  • Bergquist, now part of Henkel, is a leader in innovative and high-performance thermal management materials.

Product Range:

  • They provide advanced thermal interface materials, including high-conductivity thermal greases.

Key Features:

  • Their products are designed for demanding applications, delivering exceptional thermal performance and reliability.

Unique Selling Points:

  • Bergquist's thermal greases are suitable for high-power industrial use in Australia.

**Popular Models:

**The Bergquist Gap Filler 1000 is useful in Australian industrial setups, ensuring consistent thermal transfer across irregular surfaces, vital in fluctuating temperatures.

Availability:

  • Available on RS Australia.
Fischer Elektronik Thermal Grease

Fischer Elektronik Thermal Grease

Brand Overview:

  • Fischer Elektronik offers high-quality heat sinks and thermal management products for electronic and industrial applications, focusing on providing comprehensive thermal solutions for diverse needs.

Product Range:

  • Their thermal grease range includes a ceramic synthetic fluid thermal grease, designed to complement their heat sink solutions.

Key Features:

  • Their products offer reliability and compatibility with diverse heat sink designs, engineered for easy integration.
  • Their designs prioritise ease of use and effective thermal transfer.

Unique Selling Points:

  • Fischer Elektronik ensures reliable thermal transfer in Australian electronic applications.

Popular Models:

The Fischer Elektronik Ceramic Synthetic Fluid Thermal Grease is well-suited for high-performance applications in Australia, providing excellent thermal stability in high ambient temperatures.

Availability:

  • Available through the RS Australia online platform.
Virax Thermal Grease

Virax Thermal Grease

Brand Overview:

  • Virax provides tools and maintenance solutions, including thermal compounds tailored for various applications. They offer practical and reliable solutions for a wide range of tasks.

Product Range:

  • Their thermal greases are designed for general-purpose thermal management needs. This includes options suitable for routine maintenance and repairs.

Key Features:

  • They provide ease of use and reliability in routine maintenance, proving a practical choice for Australian professionals.

Unique Selling Points:

  • The Virax Thermal Grease is ideal for Australian maintenance professionals, with a wide operating temperature range (-30°C to +150°C) suited to Australia's climate, and a 100g tube for ample supply. This makes it a versatile and cost-effective option for various maintenance tasks.

Availability:

  • Readily available via the RS Australia site.

Safety and Handling Tips

Follow these recommended tips when applying thermal paste on a CPU for your safety and the best performance:

  • Use Gloves: Wear nitrile or latex gloves to prevent skin contact with thermal paste and avoid potential irritation.
  • Clean the CPU and Heat Sink Surface: Before application, use isopropyl alcohol and a lint-free cloth to ensure the CPU and heat sink surfaces are clean and free of debris. A clean surface will allow for optimal thermal contact and the best results.
  • Avoid Applying too Much: You only need to apply a small, pea-sized amount of thermal paste. A thin, even layer is ideal for optimal heat transfer. Using too much thermal paste can cause excess paste to ooze out and potentially cause issues.
  • Keep Thermal Paste Away from Motherboard Components: Good thermal compounds are excellent electrical conductors. While this makes them excel at heat transfer away from the CPU, the same properties can cause short circuits if the thermal paste comes into contact with sensitive motherboard components.

Final Notes on Choosing the Best Thermal Paste and Thermal Grease

Choosing the right thermal paste or thermal grease is critical for maintaining the optimal operating temperature and performance of your electronic components. Whether you're building a high-performance gaming rig, a professional workstation, or working with industrial equipment, selecting the appropriate thermal compound ensures efficient heat dissipation and prevents overheating. RS Australia is a reliable source for a diverse range of high-quality thermal management solutions from leading brands, providing the products and support you need to keep your systems running smoothly. Remember to carefully assess your specific needs, considering factors like thermal conductivity, application ease, and safety, to make an informed decision and achieve the best results.

Tip: After applying thermal paste and reassembling your system, use a fluke multimeter to test the electrical continuity and ensure all connections are secure. This step is particularly important when working with sensitive electronic components or high-power systems. This is a crucial step in ensuring the safe and effective operation of your system.

Frequently Asked Questions About Thermal Paste and Thermal Grease

Related links