- Published 10 Dec 2024
- Last Modified 10 Dec 2024
- 6 min
A Complete Guide to Electrically Erasable Programmable Read-Only Memory (EEPROM)
This guide explores what EEPROM is, how it works, and why it's a valuable memory technology in various electronic devices.

What is EEPROM?

EEPROM stands for “Electrically Erasable Programmable Read-Only Memory”.
It is a type of non-volatile memory that allows data to be stored and retrieved even when power is removed. Unlike traditional ROM (Read-Only Memory), which is permanently programmed during manufacturing, EEPROM can be erased and reprogrammed electrically, making it suitable for applications that require data updates or modifications.
EEPROM chips are commonly found in a variety of devices in Australia, including microcontrollers, memory cards, and various embedded systems. They are used to store calibration data, configuration settings, and program code that needs to be retained even when the device is powered off.
Key Features of EEPROM
EEPROM offers several key features that make it a versatile and reliable memory technology:
- Non-volatile: EEPROM retains stored data even when power is removed. This makes it suitable for applications where data persistence is essential, such as storing user settings or calibration data.
- Reprogrammable: EEPROM memory can be erased and reprogrammed electrically, allowing for in-system updates and modifications. This flexibility makes it ideal for applications that require data changes or firmware upgrades.
- Byte-Level Addressable: EEPROM allows individual bytes of data to be accessed and modified, providing granular control over data storage and retrieval.
- Low Power Consumption: EEPROM consumes minimal power, especially in standby mode, making it suitable for battery-powered and energy-efficient devices.
How EEPROM Works
Structure
EEPROM consists of a matrix of memory cells, each capable of storing a bit of data (either a 0 or a 1). These cells are organized in rows and columns.
Writing Data
To write data to an EEPROM, electrical signals are applied to the memory cells, altering their state. This programming typically uses a higher-than-normal voltage, which changes the charge on a "floating gate" inside the memory cell. This change in charge represents the binary data (0 or 1).
Erasing Data
Erasing data involves applying a higher voltage to the memory cells, removing the stored charge and returning them to their default state (usually a 1). The memory can then be reprogrammed with new data.
Accessing Data
Reading data from EEPROM is a simple process. The memory cells do not require any special voltage to read, and data can be accessed directly. This allows for quick and random access to any stored value.
Rewriting Cycles
EEPROMs have a limited number of write/erase cycles per cell (typically around 1 million) before they start to degrade. This makes them suitable for applications where data is updated occasionally rather than constantly.
There are two ways to write EEPROMs:
- Byte-wise: Data can be written or erased one byte at a time.
- Block-wise: Data is written or erased in larger blocks (e.g., 64 bytes or 256 bytes at a time).
Types of EEPROM
Serial EEPROM
Serial EEPROM is a type of EEPROM that transfers data one bit at a time, sequentially. This makes it well-suited for applications where data is accessed and updated infrequently, and where a smaller footprint and lower pin count are important.
Serial EEPROMs are commonly used in embedded systems, automotive applications, and industrial automation. They are often found in devices with limited space or power constraints, such as sensors, actuators, and small microcontrollers.
Parallel EEPROM
Parallel EEPROM, in contrast, transfers data multiple bits at a time, simultaneously, over a wider data bus. This allows for faster read and write operations, making it suitable for applications that require frequent data access or larger data transfers.
Parallel EEPROMs are often used in systems with higher performance requirements, such as industrial PCs, networking equipment, and data storage devices. However, they typically have a larger footprint and higher pin count compared to serial EEPROMs.
Flash EEPROM (or Flash Memory)
Flash EEPROM, often referred to simply as flash memory, is a variation of EEPROM that can erase and write data in blocks rather than individual bytes. This block-based operation allows for faster write speeds and makes it suitable for applications that require frequent data updates or storage of large amounts of data.
Flash memory is commonly used in USB drives, solid-state drives (SSDs), and memory cards due to its high storage capacity and relatively fast read/write speeds. However, it typically has a lower endurance (number of write/erase cycles) than traditional EEPROM.
EEPROM vs Other Types of Memory
EEPROM vs Flash Memory
EEPROM
EEPROM and flash memory are both non-volatile memory types, but they differ in how they erase and write data. EEPROM allows for byte-level erasure and programming, making it suitable for applications where individual bytes of data need to be modified, such as storing configuration data or sensor calibration values. It also typically has a higher endurance, meaning it can withstand more write/erase cycles than flash memory.
While EEPROM has a lower storage capacity than flash memory, its high endurance makes it ideal for applications where data is updated frequently.
Flash Memory
Flash memory erases and writes data in blocks, making it faster for bulk data storage and updates, such as storing firmware, operating systems, or multimedia files. Flash memory is commonly used in applications like USB drives and solid-state drives (SSDs), where large amounts of data need to be stored and accessed quickly.
However, it has a lower endurance than EEPROM and is less suitable for applications with frequent, small data updates.
EEPROM vs Flash ROM
EEPROM
EEPROM and flash ROM are both non-volatile memory types used to store persistent data. However, EEPROM allows for electrical erasure and reprogramming, making it suitable for applications where data needs to be updated or modified in-system, such as in microcontrollers.
This flexibility is crucial in devices that require firmware upgrades or store user-configurable settings.
Flash ROM
Flash ROM, while also non-volatile, is typically programmed once and cannot be easily modified after manufacturing. It is often used for storing firmware or program code in devices where updates are infrequent or performed through specialized procedures, like in gaming consoles and networking equipment.
EEPROM vs Static RAM (SRAM) and Dynamic RAM (DRAM)
EEPROM
EEPROM differs from SRAM and DRAM in its non-volatility. EEPROM retains data even when power is removed, making it suitable for storing persistent information like device settings or calibration data.
In contrast, SRAM and DRAM are volatile memory types, meaning they lose their contents when power is interrupted.
Static RAM (SRAM)
SRAM is a type of volatile memory that is faster and more power-efficient than DRAM. It is commonly used for CPU caches and embedded systems where speed and low power consumption are critical, enabling fast read/write operations for short-term data storage.
However, SRAM is more expensive and has lower storage density than DRAM.
Dynamic RAM (DRAM)
DRAM is a volatile memory type that offers high storage density at a lower cost than SRAM. It is commonly used for main memory in computers and other devices where large amounts of data need to be stored.
However, DRAM requires periodic refresh cycles to maintain data integrity and consumes more power than SRAM.
Overview of EEPROM vs Others
Memory Type | Non-volatile | Programming | Capacity | Endurance | Applications |
|---|---|---|---|---|---|
| EEPROM | Yes | Byte-level | Low | High | Config data, sensor calibration, settings storage |
| Flash Memory | Yes | Block-level | High | Moderate | Firmware, OS storage, multimedia files |
| Flash ROM | Yes | Block-level | Moderate | Moderate | Gaming consoles, networking equipment |
| SRAM | No | Fast read/write | Low | N/A | Processor caches, short-term data |
| DRAM | No | Fast read/write | Moderate | N/A | Main memory in computers |
| NOR Flash | Yes | Block-level | Moderate | High | Firmware storage, code execution |
| NAND Flash | Yes | Page/block-level | Very High | Low | SSDs, USB drives, smartphones |
Role of EEPROM in Australia
EEPROM plays a vital role in modern electronics, enabling devices to store and retain crucial data even when power is off. Its non-volatile nature and ability to be reprogrammed make it essential for various applications.
Australia's adoption of EEPROM is increasing across key sectors like industrial automation, telecommunications, and consumer electronics. This growth is driven by the rising demand for smart devices and systems that require flexible and reliable data storage.
As Australia continues to invest in the Internet of Things (IoT), smart infrastructure, and advanced electronics, the demand for EEPROM is expected to rise further. EEPROM's ability to store configuration data, calibration parameters, and sensor readings makes it a crucial component in these applications, enabling devices to operate autonomously and efficiently.
Related Product Categories
EEPROM is linked to several important product categories. Understanding EEPROM related categories helps designers choose the right memory solutions for their applications. For more related products of EEPROM, explore the offerings at RS Australia.
Related links
- Microchip Electrically Erasable Programmable Logic Device ATF16V8BQL 150 Gates 8 I/O, 62 MHz In System
- Microchip ATF16V8BQL-15XU Electrically Erasable Programmable Logic Device ATF16V8BQL 150 Gates 8 I/O, 62
- TMS320C5505AZCH12 Texas Instruments Flash, ROM 196-Pin NFBGA
- EPROM
- Chip Programmers
- CD, DVD & Blu-Ray Drives
- Renesas Electronics RL78/G13 Microcontroller 4 (Flash) kB ROM, 48-Pin LFQFP
- Renesas Electronics R5F104GCAFB#30 RL78/G14 Microcontroller 4kB FLASH 48-Pin LQFP