Moisture Meters
Moisture Meters
A moisture meter or a damp meter is a portable instrument designed for measuring the moisture levels in a range of building materials including wood, concrete, brick, and plasterboard. To learn more about moisture meters or for advice selecting the best type for your requirements, please see our moisture meters guide.
Why do we need moisture meters?
Early detection of moisture or water damage is essential. Meters help in the prevention of mould growth and structural damage, both are costly to repair and can be detrimental to health and safety.
There are two main categories of moisture metres, Pin type or Pin-less type. Both are handheld and have a screen on the front to display readings. Meters are available in a digital form with a backlit LCD display or alternatively an analogue version with a needle scale. As the meters work in slightly different ways, selecting the best one for the job at hand is dependent on the application and the environment.
Pin type
A pin-type moisture meter works by measuring the amount of electrical resistance between two points. Pin moisture meters have a pair of sharp metal pins at the top of the device. Once the metal pins are inserted into the material a small amount of electrical current is passed between the two spikes. As we all know water or moisture is a good conductor, so the higher the moisture content the lower the resistance value. The measurement is converted into a % of MC (moisture content) within the material.
Pinless type
A pinless moisture meter works by detecting how waveforms are affected by the presence of moisture in a material. The non-destructive meter works best on a flat surface. Clever internal circuitry produces a signal that is sent out through a sensing area on the back of the device. The signal is emitted in the form of electromagnetic waves. The moisture content can be converted into a scalable format to provide a moisture content reading.
Applications
Property and construction
Building inspectors use damp meters to help them identify potentially hidden hotspots behind plaster that can cause damage to structures and buildings from moisture build up.
Flooring Contractors
Being able to determine the best conditions for laying screed, concrete or wooden floors is crucial. Moisture content in materials and the relative humidity in the room must be carefully considered. Failure to do so can cause issues like distortion, cracking and buckling.
Furniture makers and woodworking
Wood naturally has a high moisture content, once dried by air or a kiln meters are used to detect moisture content ensuring the material is dry enough to work with.
Moisture Meters can help support a healthy building by improving Air Quality
Popular Searches
Related links
- Vikan Damp 42 40cm Grey Mop Head
- Uvex Orange Elastane Size 12 Aqua-Polymer Foam Coating
- LEDVANCE 9 W LED Batten Light 1 Lamp, 600 mm Long
- Uvex Uvex Athletic Black Polyamide Damp Environment Gloves NBR Coating
- Uvex Uvex Athletic Black Grey Elastane Size 11, Nitrile Micro-Foam Coating
- Uvex Uvex Athletic Black Grey Elastane Size 9, Microfoam Coating
- Uvex Uvex Athletic Black Grey Elastane Size 10, Nitrile Micro-Foam Coating
- Vikan Damp 47 40cm Grey Mop Head