Spotlights & Downlights
Spotlight and downlights are different forms of lighting typically found in ceilings in kitchens, bathrooms, living rooms and bedrooms. They are integral to providing the required light to a variety of rooms creating the perfect mood setting and enhancing your environment. Spotlights and downlights can add a touch of style and theatre turning an average space into to great space. LED spotlights and LED downlights use LED bulbs which are more energy efficient and do not emit any heat.
LED downlights
LED downlights are the perfect lighting solution for any room. They're energy-efficient, and they last for years longer than traditional incandescent bulbs. The LED technology used in each of our LED downlights is designed to provide you with the perfect amount of light for any room in your home, no matter if it's a living room or a kitchen.
LED spotlights
LED spotlights are a great way to light up your home or business. They're perfect for highlighting artwork or other important displays, as well as adding ambiance to your living room or dining area. LED spotlights are available in a range of styles and sizes, with some having adjustable heads that allow you to direct the beam of light wherever you need it most.
What is the difference between downlights and spotlights?
Downlights and spotlights are both types of lighting fixtures that can be used in residential or commercial spaces. Both types of lighting fixtures are usually used to light up a specific portion of a room, such as a dining table or a kitchen island. The only difference between the two is that downlights are recessed into the ceiling while spotlights are placed on top of the surface they're illuminating.
Types of finish
There are many different types of finish available for LED downlights and LED spotlights.
Matt White
Matt white is a very popular finish for LED downlights and LED spotlights. It’s an extremely versatile finish that can be used in any type of indoor environment, from commercial projects to residential spaces. Matt white has a sleek, modern look that works well with both contemporary and traditional designs. It’s also one of the most affordable finishes on the market.
Chrome Satin Nickel
Chrome satin nickel is another popular choice in the world of LED lights. This finish works well with both modern and traditional designs, making it perfect for use in just about any type of interior setting. The chrome satin nickel finish gives off an elegant appearance that's sure to impress everyone who sees it!
Antique Brass
If you want an antique-inspired look for your home or commercial space, then you should definitely consider purchasing antique brass-finished LEDs. These lights give off a warm glow that will instantly transport you back in time! They're also very energy efficient and easy to install.
Are they easy to install?
LED downlights
Yes, they are extremely easy to install. You just need to remove the existing light and screw in the new one. As long as you have a power point nearby, you should be able to do this job yourself without any problems.
LED spotlights
As with LED downlights, LED spotlights are also very easy to install. They are usually installed on
Popular Searches
Related links
- Facom 777.SPOTBTPB LED Work Light, IP67
- Coast HX4 LED Work Light IPX4
- HPM LWK0110WBL LED Work Light 230-240 V, IP44
- HPM LWK0220WBL LED Work Light 230-240 V, IP44
- Schneider Electric IMT47223 LED Work Light 230 V, IP65
- Schneider Electric IMT47210 LED Work Light 230 V, IP65
- HPM LWK0130WBL LED Work Light 230-240 V, IP44
- HPM LWK0240WBL LED Work Light 230-240 V, IP44