Medical Lights
Medical Lights are crucial for providing enough illumination in poorly lit areas, such as near the wash basin in an operating room or bedside table. Medical Lights are also commonly used for illuminating a patient when diagnostics and treatments of the eyes, such as in the pupil examination, a vital step to prevent eye diseases.
This article will discuss several different types of medical lights. There are a lot of uses for them in the healthcare setting, and knowing about the various available options can come in handy.
Surgical Headlight
A surgical headlight is a device used in surgeries and other medical procedures to provide illumination. It is a type of surgical instrument that has a built-in light source.
The surgical headlight is attached to the head of the surgeon, and it can provide enough light for them to see clearly during surgery. It is also helpful for other medical practitioners, such as nurses, dentists, and dental hygienists who work in dark areas or places with no lights.
Types of Medical Lights
Medical lights come in different types, each with a special use in the medical room. They include:
Surgical Lights
Surgical lights are used for illumination during surgery and are generally powered by various methods. In the past, surgical lights were powered by large-scale generators, which provided a more even light across the room. Nowadays, surgical lights can be powered by batteries or portable generators. These small generators can be used in hospitals to increase the efficiency of surgeries while also reducing costs. Surgeries use these lights because they provide a clear view of the area being operated on so that surgeons can work more precisely and effectively.
Penlights
A penlight is a small hand-held flashlight used for the general vision examination. Penlights typically have a small lens that shines into the eye from one side or top of the device. They are also called ophthalmoscopes because they can be used to examine both the outside structure and inside structures of the eye (the retina). Penlights come in many sizes and colors but most commonly feature black or white color schemes.
Medical Exam Lights
These lights are compact and portable, making them easy to move around the room or exam table. These lights are not used for surgery or other invasive procedures but general examinations or minor surgeries. They often have a magnifying lens attached to them so that you can get a closer look at your patient’s skin or any other area you need to examine.
Woods Lights
Woods lights are larger versions of medical exam lights that include an attachment for an oscillating arm so that it can be placed over your patient’s body without touching them directly. This way, you do not have to worry about being hit by an oscillating arm when trying to treat your patient.
Most of these medical lights are great for the intended use. They are well made to ensure they last and benefit the people who need them in their everyday lives.
Related links
- EDL Lighting Limited Incandescent Medical Light Reach:1100mm 230 V ac
- Ceratech Wired USB Medical Touchpad Keyboard Black
- Ceratech Wired USB Medical Touchpad Keyboard White
- Ceratech AccuMed 5 Button Wireless Medical Optical Mouse White
- Ceratech AccuMed 5 Button Wired Medical Optical Mouse Black
- Leatherman 127 mm Stainless Steel Medical Scissors
- Kimberly Clark Pad Spill Absorbent for Medical Use, 100 per Pack